N9038B MXE EMI Receiver

Data Sheets

Definitions and Conditions

 

Specifications describe the performance of parameters covered by the product warranty and apply to the full temperature range of 0 to 55 °C, unless otherwise noted.

 

95th percentile values indicate the breadth of the population (approx. 2 σ) of performance tolerances expected to be met in 95 percent of the cases with a 95 percent confidence, for any ambient temperature in the range of 20 to 30 °C. In addition to the statistical observations of a sample of instruments, these values include the effects of the uncertainties of external calibration references. These values are not warranted. These values are updated occasionally if a significant change in the statistically observed behavior of production instruments is observed.

 

Typical describes additional product performance information that is not covered by the product warranty. It is performance beyond specifications that 80 percent of the units exhibit with a 95 percent confidence level over the temperature range  20 to 30 °C. Typical performance does not include measurement uncertainty.

 

Nominal values indicate expected performance, or describe product performance that is useful in the application of the product, but are not covered by the product warranty.

 

The receiver will meet its specifications when:

 

• It is within its calibration cycle

• Under auto couple control, except when Auto Sweep Time Rules = Accy

• Signal frequencies < 10 MHz, with DC coupling applied

• The receiver has been stored at an ambient temperature within the allowed operating range for at least two hours before being turned on

• The receiver has been turned on at least 30 minutes with Auto Align set to normal, or, if Auto Align is set to off or partial, alignments must have been run recently enough to prevent an Alert message; if the Alert condition is changed from “Time and Temperature” to one of the disabled duration choices, the receiver may fail to meet specifications without informing the user

 

This data sheet is a summary of the specifications and conditions for the MXE EMI receiver. For the complete specifications guide, visit: www.keysight.com/find/mxe_specifications

 

Keep the test queue flowing

 

In EMC testing, success depends on tools that can help you do more in less time—today and tomorrow. That’s why Keysight Technologies, Inc. created the MXE: it’s a standards-compliant EMI receiver and diagnostic signal analyzer built on an upgradeable platform. In the lab and on the bench, it provides the accuracy, repeatability, and reliability you need to test with confidence. Equip your team with the MXE, and keep the test queue flowing.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.