Keysight Collaborates with Nokia to Demonstrate the First 800 Gigabit Ethernet Readiness and Interoperability Public Test

Enables network operators to validate the reliability of high bandwidth and scale 800 Gigabit Ethernet (GE) in service provider and data center environments

SANTA ROSA, Calif., August 3, 2022 

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced it has collaborated with Nokia to successfully demonstrate the first public 800GE test, validating the readiness of next-generation optics for service providers and network operators.

With the move to the 800GE pluggable optics on front panel ports, interconnect and link reliability requires a new round of validation cycles to support carrier-class environments. These high-speed interfaces create a unique challenge as new 800GE capable silicon devices, optical transceivers and high bandwidth Ethernet speeds must be accurately tested.

The readiness testing was conducted at Nokia's private SReXperts customer event in Madrid in June 2022, and included Keysight's AresONE 800GE Layer 1-3 800GE line rate test platform and the Nokia 7750 Service Routing platform. The AresONE was used to test and qualify Nokia's FP5 network processor silicon along with 800GE pluggable optics. Specific Nokia platforms used in the validation were the FP5 based 7750 SR-1x-48D supporting 48 ports of 800GE and the 7750 SR-1se supporting 36 ports of 800GE.

Nokia's FP5 silicon delivers 112G SerDes which enables 800GE support in hardware. FP5 enables networks to efficiently scale capacity and concurrently IP subscriber services while maintaining integrity, providing advanced protection against escalating network security threats, and lowering power consumption. Nokia is the first vendor to ship high-density 800GE systems this year with platforms supporting a range of 36 x 800GE in compact fixed platforms to 432 ports of 800GE in the flagship 7750 SR-14s.

"The move to 800GE presents service providers and vendors in the supply chain with new challenges to validate chips, optical transceivers, or networking equipment port electronics," said Ram Periakaruppan, vice president and general manager, Keysight's Network Test and Security Solutions group. "The unique combination of the Keysight AresONE 800GE test system and Nokia's 7750 Service Router addresses the interoperability challenges in 112Gbps electrical lane signaling and supports the service provider community to accelerate validation of carrier-class 800GE devices and network infrastructure in a multi-service environment."

"We are extremely pleased to partner with Keysight and showcase our FP5 silicon in this important, world's first demonstration," said Ken Kutzler, vice president of IP Routing Hardware at Nokia. “Nokia's industry leading, innovative FP5 silicon is the first network processor silicon for high-performance routing to meet the demands of the 800GE network upgrade cycle. The combination of Keysight's AresONE 800GE with Nokia's FP5 and 7750 SR platform meets both the performance and verification needs of our 800GE IP routing interfaces." 

About Keysight Technologies   

Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight's dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow's technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics markets. Keysight generated revenues of $4.9B in fiscal year 2021. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.

Keysight Contact:

Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com