What are you looking for?
Keysight’s 64 GBaud Bit Error Ratio Tester Secures PCI-SIG Approval for Compliance Test Measuring of PCIe 4.0 Technology
Supports PCIe 5.0 testing and pathfinding for emerging PCIe 6.0 standard
SANTA ROSA, Calif. March 17, 2021
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that delivers advanced design and validation solutions to help accelerate innovation to connect and secure the world, announced that the company's M8040A 64 Gbaud High-performance bit error ratio tester (BERT) was approved by the PCI-SIG as a compliance test measuring instrument for PCI Express 4.0 (PCIe Gen4) testing at 16 gigatransfers per second (GT/s) and 8GT/s. Keysight is the only test vendor with two BERT systems approved by the PCI-SIG for testing PCIe 4.0 and PCIe 3.0 technologies.
As serial bus technologies increase in speed and bandwidth, test equipment vendors are tasked with delivering tools capable of testing beyond the state of the art. Keysight's BERT system enables accurate physical-layer design verification of high-speed communication and multigigabit digital interfaces. Keysight M8040A 64 Gbaud High-performance BERT is the only PCI-SIG approved receiver test BERT for PCIe 4.0 capable of testing PCIe 5.0 (32GT/s) and enables pathfinding (the process of selecting a design choice by evaluating different technical approaches against a set of defined system parameters and goals) for the emerging PCIe 6.0 (64GT/s) speeds.
"The PCI-SIG is very pleased to have Keysight participate as one of the key test vendors it relies on to provide effective compliance testing to our members at its official workshops," said Al Yanes, chairman of the PCI-SIG. "We appreciate the time, effort and expense associated with our test events and recognize Keysight's continued support of SIG activities, especially obtaining approval for the equipment that is used for official compliance testing."
"Keysight is pleased to receive PCI-SIG's approval of the M8040A high performance BERT for PCIe 4.0 receiver testing," said Kailash Narayanan, vice president for Keysight's commercial communications group. "The PCI Express standard is important to Keysight and our customers. As the industry looks ahead to PCIe 6.0, we believe that approval of our M8040A for PCIe 4.0 receiver testing will enhance our customers confidence in test tools that can be used today while offering a clear runway to next generation technologies at speeds up to 32Gbaud PAM4."
"PCI Express based I/O technology is expected to set the lead for high-performance I/O interfaces including accelerator interconnects like Compute Express Link," said Jim Pappas, Director of Technology Initiatives, Intel Corporation. "Receiver and transmitter test solutions from companies including Keysight Technologies are critical to enabling the development, deployment and adoption of high performance I/O technologies on future Intel platforms and throughout the industry."
The PCI-SIG (originally formed as the Peripheral Component Interconnect Special Interest Group) develops and manages the PCI bus specification, the industry standard for a high-performance I/O interconnect for transferring data between central processing units and peripherals. Currently, the PCI-SIG manages the PCI, PCI-X® and PCI Express standards.
The PCI-SIG continues to evolve the PCI standard to meet the industry's needs. Through interoperability testing, technical support, seminars and industry events, the PCI-SIG enables its members to generate competitive and quality products.
Additional Information about Keysight's high speed digital system design solutions is available at https://www.keysight.com/us/en/solutions/high-speed-digital-system-design.html
About Keysight Technologies
Keysight delivers advanced design and validation solutions that help accelerate innovation to connect and secure the world. Keysight’s dedication to speed and precision extends to software-driven insights and analytics that bring tomorrow’s technology products to market faster across the development lifecycle, in design simulation, prototype validation, automated software testing, manufacturing analysis, and network performance optimization and visibility in enterprise, service provider and cloud environments. Our customers span the worldwide communications and industrial ecosystems, aerospace and defense, automotive, energy, semiconductor and general electronics. Keysight generated revenues of $4.2B in fiscal year 2020. For more information about Keysight Technologies (NYSE: KEYS), visit us at www.keysight.com.
Intel, the Intel logo, and other Intel marks are trademarks of Intel Corporation or its subsidiaries.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter, and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662–4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com
Caption: Keysight 64 GBaud Bit Error Ratio Tester
Need to contact Media Relations at Keysight?