您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

主要技術規格

  • Adds front handles to the instrument

敘述

Install Handles on the Front of the PSG

The PSG equipped with Option 1CN supplies a front handle kit, which contains a pair of handles and the necessary hardware to attach them to the front of the signal generator. If you want to install handles and rackmount the signal generator into a cabinet, refer to Option 1CP (rackmount flange and front handle kit).