您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

主要技術規格

  • Adds front handles to the instrument

敘述

Install Handles on the Front of the ESG

Option 1CN supplies a front handle kit with the necessary hardware to attach two handles on the front of the signal generator.

This kit is not for use in rackmount environments. If you want to install handles and mount the ESG into a rack or cabinet, refer to Option 1CP (Rackmount Flange and Front Handle Kit).

This option can be added as a product upgrade.