Choose a country or area to see content specific to your location
- 產品概述與特色
- 採購後升級選項
- 資源
HIGHLIGHTS
Note: Model number 85190M-020 has been obsoleted; however, the feature/capability is now included in the E8900K-030.
The information below is provided for reference only.
The universal serial bus (USB) Port Hardware Key secures IC-CAP software licenses by enabling IC-CAP to run on a personal computer (PC) in which this key is plugged into.
Upon your purchase of IC-CAP, your IC-CAP license file can be generated using either:
- the unique 9 digit serial number of the USB Port Hardware key (as shown), or...
- the local area network (LAN) Ethernet (wired or wireless) adapter's physical address
The USB Port Hardware key offers the convenience of IC-CAP license portability to run IC-CAP on different computers where IC-CAP and its license file are installed. However, you may risk losing this USB key which then prevents you from using IC-CAP.
To avoid this situation, you can alternatively secure your IC-CAP license to your PC LAN physical address. In this case, the USB Port Hardware Key would not be required.
Note: Keysight does not recommend the usage of the USB Port Hardware Key for machines used to run automated measurements via IC-CAP.