您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

無線網路模擬器

利用是德科技產品,行動電話設計業者和製造商可用更快的量測速度、更高的準確度,以及絕佳的靈活度,來測試行動裝置。我們的單機式測試儀可因應所有主要技術格式:LTE-Advanced, LTE(FDD 和 TDD)、GSM/GPRS/EGPRS/E-EDGE、W-CDMA/HSPA/HSPA+/DC-HSDPA、cdma2000®/1xEV-DO/eHRPD、TD-SCDMA/TD-HSDPA/TD-HSUPA、IS-95、TIA/EIA-136、AMPS、Bluetooth®、Bluetooth Enhanced Data Rate(EDR)、Bluetooth Low Energy、ZigBee™、Wireless LAN(WLAN)、802.11a/b/g、802.11n、NFC/EMV、MIMO 和 WiMAX™。

您可使用是德科技軟體產品擴充無線測試儀的功能,以便加速完成無線量測,並透過自動化測試功能完成耗時且複雜的量測分析任務。所有無線通訊測試儀平台皆可使用上述軟體,針對蜂巢式行動裝置、WiMAX、LTE 和 Bluetooth/WLAN 裝置進行自動化測試。

是德科技系統將儀器、佈線和系統硬體,整合入兼顧散熱、電源、人體工學、安全性和機械穩定性的機架中。讓是德科技協助您輕鬆、快速地處理設計到量產的所有量測任務,同時降低測試成本,讓您更快達到預期的收益。

Anite 的相關解決方案

是德科技新近購併了 Anite。Anite 的裝置和基礎設施測試事業群現在由是德科技統領。請瀏覽以下資訊,以獲得 Anite 相符性工具套件、Anite SAS 互通性測試、Propsim 通道模擬解決方案、Anite 虛擬路測工具套件和 Anite 開發工具套件的詳細資訊。請瀏覽 www.anite.com ,以獲得 Anite 網路測試部門與其 Nemo 品牌解決方案的相關資訊。

1-25 / 414

排序:
E7515A UXM Wireless Test Set Getting Started Guide
This manual documents UXM software

使用手冊 2019-08-01

PDF PDF 3.21 MB
E7515B UXM 5G Wireless Test Set Getting Started Guide
This manual provides a “Quick Start” introduction to the E7515B UXM 5G Test Set, its front and rear panel functions, its Control Panel application, its operating system, and its Internal Applications Server.

使用手冊 2019-08-01

PDF PDF 4.87 MB
E6640A EXM Wireless Test Set Getting Started Guide
Getting started information for the E6640A EXM wireless test set.

使用手冊 2019-07-01

PDF PDF 6.93 MB
E7760B Wideband Transceiver Getting Started Guide
Safety information, basic instructions for use, operating tasks, and an introduction to the user interface and operating system.

使用手冊 2019-01-01

PDF PDF 5.71 MB
E7515B UXM 5G Firmware Update Tool Installation & User Guide
Instructions on how to update the firmware of E7515B UXM 5G units.

使用手冊 2018-12-01

PDF PDF 1.31 MB
E7760A Wideband Transceiver User's Guide
Instructions on how to use the 5G test application with the E7760B Wideband Transceiver.

使用手冊 2018-11-01

PDF PDF 7.51 MB
M1740A mmWave Transceiver Getting Started Guide
Getting started information for the M1740A mmWave Transceiver.

使用手冊 2018-10-01

PDF PDF 1.28 MB
E7530A LTE/LTE-A Test Application Online Documentation (.chm)
This help describes how to use the E7530A LTE/LTE-A Test Application for software revision 1.9.1.0. You must copy this file to your PC (or the UXM) in order to view its contents.

輔助說明檔 2018-08-16

CHM CHM 1.64 MB
Signal Studio Waveform Licenses User's Guide
Use the N76xxB Signal Studio software to configure, generate, and download waveform files to your instrument.

使用手冊 2018-01-01

PDF PDF 580 KB
E7515A UXM Wireless Test Set User's and Programmer's Guide
This manual describes the following aspects of the E7515A UXM: - using the Application Switch Tool - setting up the programming connection for sending SCPI commands to each UXM software component - specifying RF Cable Compensation.

使用手冊 2017-12-01

E7760A Wideband Transceiver User's Guide
A guide to the screen interface and SCPI programming interface for the E7760A. Also: test scenarios, port usage, and information on the IEEE 802.11ad-2012 PHY radio standard.

使用手冊 2017-07-01

PDF PDF 12.44 MB
X-Series Multi-touch Test Set User Documentation (webhelp)
Online documentation that includes programming information, SCPI commands, and more.

輔助說明檔 2017-06-05

E7760A Wideband Transceiver Getting Started Guide
Safety information, basic instructions for use, operating tasks, and an introduction to the user interface and operating system.

使用手冊 2017-05-01

PDF PDF 4.67 MB
E7521A GSM/GPRS/EGPRS Test Application Online Documentation (.chm)
This help describes how to use the E7521A GSM/GPRS/EGPRS Test Application for software revision 1.6.1.x. You must copy this file to your PC (or the UXM) in order to view its contents.

輔助說明檔 2017-03-01

CHM CHM
E7523A W-CDMA Test Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the E7523A W-CDMA software applications. Refer to the topic: Using Help > Updating the Help File in this chm for instructions for replacing the context-sensitive help in your UXM. You must copy this file to your PC (or the UXM) in order to view its contents. system functions, and measurement functions.

輔助說明檔 2017-03-01

E7515A UXM Firmware Update Tool Installation and User Guide
Instructions and user information on how to use the E7515A firmware update tool.

使用手冊 2017-03-01

PDF PDF 672 KB
E7529A TD-SCDMA/HSPA Test Application Online Documentation (.chm)
This help describes how to use the E7529A TD-SCDMA/HSPA Test Application for software revision 1.6.1.x. You must copy this file to your PC (or the UXM) in order to view its contents.

輔助說明檔 2016-12-06

CHM CHM
M1650A mmWave Transceiver Getting Started Guide
Safety information, location and mounting, and exterior connections for the M1650A, which is used as a test head for the E7760A Wideband Transceiver.

使用手冊 2016-10-01

PDF PDF 277 KB
Protocol Logging and Analysis Software (E7515A-L01) - User Guide
Installation and user information for the Protocol Logging & Analysis software. You must have this license (E7515A-L01) to capture data from the UXM

使用手冊 2016-09-01

PDF PDF 3.29 MB
Remote Radio Head Tester E6610A - User and Programming Guide
User and Programming Guide for the E6610A Remote Radio Head Tester

使用手冊 2016-09-01

PDF PDF 3.76 MB
E6610A Remote Radio Head Tester Startup Guide
Start-up information for the E6610A remote radio head tester.

使用手冊 2016-08-01

PDF PDF 15.03 MB
T9080B LTE/ LTE-A FDD X-Series Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the LTE/LTE-A FDD mode of the LTE/LTE-A X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or to the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

輔助說明檔 2016-04-01

CHM CHM 10.79 MB
T9082B LTE TDD/LTE-A TDD X-Series Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the LTE/LTE-A TDD mode of the LTE/LTE-A X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or to the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

輔助說明檔 2016-04-01

CHM CHM 10.80 MB
T9079A TDSCDMA with HSPA8PSK Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the TDSCDMA mode of the 2G/3G X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

輔助說明檔 2016-04-01

T9073B W-CDMA & HSPA Measurement Applications User’s & Programmer’s Reference Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the W-CDMA mode of the 2G/3G X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

輔助說明檔 2016-04-01

1 2 3 4 5 6 7 8 9 10 ... 下一頁

相關產業與技術