这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

没有可替代产品

主要特性与技术指标

  • Provides RS-232 and GPIB connectivity
  • Outputs results of pass/fail (limit) testing
  • Provides remote control using the 3000 Series´ SCPI command set.

Also allows PC connectivity via free Scope Connect Software

描述

The N2861A communications module fits easily onto the back panel of your 3000 Series oscilloscope. 3000 Series oscilloscope users who wish to use the native SCPI programming command set must use the N2861A´s RS-232 or GPIB ports.

Note: The DSO3000 series command set is not a "drop in" replacement for other Keysight oscilloscopes. Some command translation and conversion will be required.

For more information on: Scope Connect Software