这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

功率计 + 功率传感器

是德科技功率计可与多种传感器结合使用(连续波、平均功率和峰值功率传感器),覆盖多个频率和功率范围,能够精确地测量射频和微波信号的功率。应用包括:测试通信基站发射机、蜂窝电话、雷达系统设备及其他设备的输出功率。

了解如何选择最适当的功率计和功率传感器:《功率计和传感器选型指南》

Microwaves and RF’s

是德科技被《Microwaves and RF》读者评选为“2013 年最佳供应商社交媒体”。这个奖项旨在表彰 2013 年在为工程师提供关键信息方面表现优异的供应商。

比较所有的功率计和功率传感器 (51)

缩小范围

去除所有优化

按内容类型

按产品类别

1-4 / 4

排序:
DAQ with Matlab for Medical Science - Case Study
Keysight data acquisition (DAQ) units can now work with MATLAB in medical research, as illustrated by the case study. This helps users to understand the basics of MATLAB programming in Keysight USB DAQ.

案例分析 2009-06-16

PDF PDF 164 KB
New USB Power Sensor Technology Uses Digitized Data To Provide Versatile Power Measurement
This article covers the digitizing technology behind each U2000 Series USB power sensor

文章 2007-05-01

Measuring Power Levels in Modern Communications Systems
This article explores the types of power measurements required by third-generation (3G) wireless communications systems, and highlights the contribution to the measurement accuracy that can be made by a properly designed test system.

文章 2002-06-19

Use A Sampling Power Meter To Determine The Characteristics of RF and Microwave Devices
This two-part article discusses triggering, data acquisition and peak-mode measurements using a sampling power meter

文章 2002-04-09