这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

无线网络仿真器

是德科技产品为手机设计人员和制造商提供了更快的测量速度、更高的精度和出色的灵活性,使他们能够更好地测试移动设备。我们的综合测试仪涵盖所有主要的技术制式:LTE-Advanced、LTE (FDD 和 TDD)、GSM/GPRS/EGPRS/E-EDGE、W-CDMA/HSPA/HSPA+/DC-HSDPA、cdma2000®/1xEV-DO/eHRPD、TD-SCDMA/TD-HSDPA/TD-HSUPA, IS-95、TIA/EIA-136、AMPS、蓝牙®、蓝牙 增强数据速率(EDR)、蓝牙 低能量、ZigBee™、无线局域网(WLAN)、802.11a/b/g、802.11n、NFC/EMV、MIMO 和 WiMAX™。

此外,我们的软件产品进一步扩展了是德科技无线测试仪的功能,这些产品可以简化无线测量,自动完成耗时而复杂的测量和分析任务。软件产品适用于所有无线通信测试仪平台――自动测试蜂窝移动设备、WiMAX、LTE 和蓝牙/WLAN 设备。

是德科技系统将仪器、布线和系统硬件集成到一个机架中,可提供出色的散热性能、电力供应、人体工程学设计、安全性和机械稳定性。是德科技帮助您简化从设计到批量生产的过渡,降低测试成本,进而更快地实现盈利。

Anite 提供的相关解决方案

Anite 现在已成功融入是德科技。Anite 的设备和基础设施测试业务现在在是德科技的旗下开展工作。请了解下面关于 Anite 一致性测试工具套件、Anite SAS 互操作性测试、Propsim 信道仿真解决方案、Anite 虚拟路测工具套件和 Anite 开发工具套件的信息。有关 Anite 网络测试业务及其 Nemo 品牌解决方案的更多信息,请访问 www.anite.com 

1-25 / 415

排序:
E7515A UXM Wireless Test Set Getting Started Guide
This manual documents UXM software

用户手册 2019-08-01

PDF PDF 3.21 MB
E7515B UXM 5G Wireless Test Set Getting Started Guide
This manual provides a “Quick Start” introduction to the E7515B UXM 5G Test Set, its front and rear panel functions, its Control Panel application, its operating system, and its Internal Applications Server.

用户手册 2019-08-01

PDF PDF 4.87 MB
E6640A EXM Wireless Test Set Getting Started Guide
Getting started information for the E6640A EXM wireless test set.

用户手册 2019-07-01

PDF PDF 6.93 MB
E7760B Wideband Transceiver Getting Started Guide
Safety information, basic instructions for use, operating tasks, and an introduction to the user interface and operating system.

用户手册 2019-01-01

PDF PDF 5.71 MB
E7515B UXM 5G Firmware Update Tool Installation & User Guide
Instructions on how to update the firmware of E7515B UXM 5G units.

用户手册 2018-12-01

PDF PDF 1.31 MB
E7760A Wideband Transceiver User's Guide
Instructions on how to use the 5G test application with the E7760B Wideband Transceiver.

用户手册 2018-11-01

PDF PDF 7.51 MB
M1740A mmWave Transceiver Getting Started Guide
Getting started information for the M1740A mmWave Transceiver.

用户手册 2018-10-01

PDF PDF 1.28 MB
E7530A LTE/LTE-A Test Application Online Documentation (.chm)
This help describes how to use the E7530A LTE/LTE-A Test Application for software revision 1.9.1.0. You must copy this file to your PC (or the UXM) in order to view its contents.

帮助文件 2018-08-16

CHM CHM 1.64 MB
Signal Studio Waveform Licenses User's Guide
Use the N76xxB Signal Studio software to configure, generate, and download waveform files to your instrument.

用户手册 2018-01-01

PDF PDF 580 KB
E7515A UXM Wireless Test Set User's and Programmer's Guide
This manual describes the following aspects of the E7515A UXM: - using the Application Switch Tool - setting up the programming connection for sending SCPI commands to each UXM software component - specifying RF Cable Compensation.

用户手册 2017-12-01

E7760A Wideband Transceiver User's Guide
A guide to the screen interface and SCPI programming interface for the E7760A. Also: test scenarios, port usage, and information on the IEEE 802.11ad-2012 PHY radio standard.

用户手册 2017-07-01

PDF PDF 12.44 MB
X-Series Multi-touch Test Set User Documentation (webhelp)
Online documentation that includes programming information, SCPI commands, and more.

帮助文件 2017-06-05

E7760A Wideband Transceiver Getting Started Guide
Safety information, basic instructions for use, operating tasks, and an introduction to the user interface and operating system.

用户手册 2017-05-01

PDF PDF 4.67 MB
E7521A GSM/GPRS/EGPRS Test Application Online Documentation (.chm)
This help describes how to use the E7521A GSM/GPRS/EGPRS Test Application for software revision 1.6.1.x. You must copy this file to your PC (or the UXM) in order to view its contents.

帮助文件 2017-03-01

CHM CHM
E7523A W-CDMA Test Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the E7523A W-CDMA software applications. Refer to the topic: Using Help > Updating the Help File in this chm for instructions for replacing the context-sensitive help in your UXM. You must copy this file to your PC (or the UXM) in order to view its contents. system functions, and measurement functions.

帮助文件 2017-03-01

E7515A UXM Firmware Update Tool Installation and User Guide
Instructions and user information on how to use the E7515A firmware update tool.

用户手册 2017-03-01

PDF PDF 672 KB
E7529A TD-SCDMA/HSPA Test Application Online Documentation (.chm)
This help describes how to use the E7529A TD-SCDMA/HSPA Test Application for software revision 1.6.1.x. You must copy this file to your PC (or the UXM) in order to view its contents.

帮助文件 2016-12-06

CHM CHM
M1650A mmWave Transceiver Getting Started Guide
Safety information, location and mounting, and exterior connections for the M1650A, which is used as a test head for the E7760A Wideband Transceiver.

用户手册 2016-10-01

PDF PDF 277 KB
Protocol Logging and Analysis Software (E7515A-L01) - User Guide
Installation and user information for the Protocol Logging & Analysis software. You must have this license (E7515A-L01) to capture data from the UXM

用户手册 2016-09-01

PDF PDF 3.29 MB
Remote Radio Head Tester E6610A - User and Programming Guide
User and Programming Guide for the E6610A Remote Radio Head Tester

用户手册 2016-09-01

PDF PDF 3.76 MB
E6610A Remote Radio Head Tester Startup Guide
Start-up information for the E6610A remote radio head tester.

用户手册 2016-08-01

PDF PDF 15.03 MB
T9080B LTE/ LTE-A FDD X-Series Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the LTE/LTE-A FDD mode of the LTE/LTE-A X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or to the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

帮助文件 2016-04-01

CHM CHM 10.79 MB
T9082B LTE TDD/LTE-A TDD X-Series Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the LTE/LTE-A TDD mode of the LTE/LTE-A X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or to the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

帮助文件 2016-04-01

CHM CHM 10.80 MB
T9079A TDSCDMA with HSPA8PSK Measurement Application Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the TDSCDMA mode of the 2G/3G X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

帮助文件 2016-04-01

T9073B W-CDMA & HSPA Measurement Applications User’s & Programmer’s Reference Help (.chm file)
This Help file describes the settings and remote programming commands (SCPI) for the W-CDMA mode of the 2G/3G X-Series Application of the E7515A UXM Test Set. You must copy this file to your PC (or the Test Set) in order to view its contents. To replace the current version of this help file in your Test Set, copy this file to the location listed under the Help topic: Using Help.

帮助文件 2016-04-01

1 2 3 4 5 6 7 8 9 10 ... 下一页

相关行业和技术