这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

自动 X 射线检测

是德正在退出自动光学检测和自动 x 射线检测业务。是德将会遵守现有的保修和支持合同,在支持期满前继续为客户提供备用部件、时间和材料服务和自我支持选件。产品的支持期限为停产后七年,从 2009 年 3 月 1日算起。

有关该退出声明的常见问题解答列表,请访问: www.keysight.com/find/inspection.

不过,是德仍将全力以赴扩展其在印刷电路板组装测试市场中的在线测试(ICT)功能测试产品系列。

51-60 / 60

排序:
Series II Compliance with the Machinery Directive (in Europe) - specific installation procedures
Series II will meet requirements of Machinery Directive in European Community member countries, if the following steps, which are described in the document, are taken during installation of equipment.

应用说明 2001-05-17

Dealing with Board Thickness Variations
The Keysight 5DX has the capability to be implemented such that it can accommodate thickness variations on a board-by-board basis. NOTE: Content described is in the 5DX Reference Guide but is no longer in Chapter 7 as mentioned herein.

应用说明 2001-05-16

PDF PDF 31 KB
Improved Fault Coverage in a Combined X-ray and In-Circuit Test Environment
Cutting functional test failures in half and doubling the faults detected at process test! These are some of the case study results observed in combined X-ray and in-circuit test environments.

应用说明 2001-02-27

PDF PDF 575 KB
Use of Wrong Thickness Technique Gives Bad Test Results
Beginning with release 6.0, there are two techniques for measurement of solder thickness on the Keysight 5DX, each based on use of a different Confirmation & Adjustment panel.

应用说明 2000-12-31

Learned Data for the 5DX
The Keysight 5DX uses learned data in several ways to improve algorithm performance. There are basically 2 different forms of learned data.

应用说明 2000-11-01

The Why, Where, What, How, and When of X-ray Test
How do the different AXI technologies work? What are the appropriate uses of 2D vs 3D X-ray? Where in the mfg process should AXI be placed? How can AXI be used to improve the mfg process?

应用说明 2000-11-01

PDF PDF 1.30 MB
Reducing Load Time for Loaderless Systems
For Series 2L systems, it may be possible to reduce the time it takes to load a panel.

应用说明 1999-12-01

NDF and RTF - Hashed Names
There have been many questions about hashed directory names. This is a brief explanation of why they are, and how they are generated.

应用说明 1998-06-30

Effects of Lead Free Solders on Imaging Characteristics of the Keysight 5DX Laminographic X-ray Test
The electronics industry is under pressure to migrate solder processes away from the usage of eutectic tin-lead solder and towards utilization of lead-free compounds.

应用说明 1998-05-01

PDF PDF 83 KB
Use of the Test Results Command Processor
TRCMDPRO processes the results from the Keysight 5DX in a way that is specified by a command file. This file is TRCMDPRO.CMD. In addition to the software revisions named, the document applies to all 5DX software versions.

应用说明 1998-01-12

PDF PDF 20 KB

以前 1 2 3