这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

自动 X 射线检测

是德正在退出自动光学检测和自动 x 射线检测业务。是德将会遵守现有的保修和支持合同,在支持期满前继续为客户提供备用部件、时间和材料服务和自我支持选件。产品的支持期限为停产后七年,从 2009 年 3 月 1日算起。

有关该退出声明的常见问题解答列表,请访问: www.keysight.com/find/inspection.

不过,是德仍将全力以赴扩展其在印刷电路板组装测试市场中的在线测试(ICT)功能测试产品系列。

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

1-9 / 9

排序:
Quad Flat No Lead (QFN) Best Practices
The purpose of this application note and best practices guide is to describer the QFN-type component and provide testing methods to ensure robust testing on the Medalist 5DX Automated X-ray Inspection (AXI) System.

应用说明 2008-08-26

PDF PDF 492 KB
Tips for X-ray Users On Exporting NDF’s With No Loads Set To False
Navigating CAD can be a time consuming process. Small tips can be extremely helpful in creating quality programs in a short amount of time.

应用说明 2007-10-18

X-ray Test Users Utilize BOM Explorer to Change
Automated X-ray Inspection 5DX Users can save time by implementing these quick and easy steps to use BOM explorer to change "no pops" to "untested".

应用说明 2007-10-12

Test and Inspection as Part of the Lead-free Manufacturing Process
The paper addresses issues that will impact defect levels and defect spectrum during the transition to lead-free manufacturing. It also addresses different test and inspection systems’ readiness to test lead-free printed circuit board assemblies.

应用说明 2005-02-22

PDF PDF 421 KB
The Importance of Test and Inspection When Implementing Lead-Free Manufacturing
Many papers, articles, and studies have been written about process issues, reliability issues, repair issues, and the merits of different alloys. This paper addresses the impacts on test and inspection when going lead-free.

应用说明 2004-08-20

PDF PDF 260 KB
What to Consider When Selecting the Optimal Test Strategy
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

应用说明 2003-03-01

PDF PDF 175 KB
Comparing AOI and AXI
Choosing the right technology requires looking at board mix, capital budget and other business considerations. But most of all, you need to understand the typical characteristics of each technology.

应用说明 2001-07-25

PDF PDF 42 KB
Series II Compliance with the Machinery Directive (in Europe) - specific installation procedures
Series II will meet requirements of Machinery Directive in European Community member countries, if the following steps, which are described in the document, are taken during installation of equipment.

应用说明 2001-05-17

Improved Fault Coverage in a Combined X-ray and In-Circuit Test Environment
Cutting functional test failures in half and doubling the faults detected at process test! These are some of the case study results observed in combined X-ray and in-circuit test environments.

应用说明 2001-02-27

PDF PDF 575 KB