这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Discontinued Miscellaneous

Other Accessories

  • 18356-98201 ISDN 基础 18356-98201 ISDN 基础 

    18356-98201 ISDN 基础

    The ISDN 基础手册是 ISDN(综合业务数字广播)的概述, 旨在帮助您熟悉 ISDN。

  • E3943B IS08882 X.25 CTS [已淘汰] E3943B IS08882 X.25 CTS [已淘汰] 

    E3943B IS08882 X.25 CTS [已淘汰]

    X.25 ISO 8882 3rd Edition DIS Test Suite

  • J2295A Keysight Advisor - PC Empty Undercradle  [已淘汰] J2295A Keysight Advisor - PC Empty Undercradle [已淘汰] 

    J2295A Keysight Advisor - PC Empty Undercradle [已淘汰]

    Keysight Advisor - PC undercradle allows up to two full-sized PC AT cards to be added and operated by the 486-based Keysight Advisor Series.

  • J2530A Token Ring-Parallel Port Adapter (North American Power) [已淘汰] J2530A Token Ring-Parallel Port Adapter (North American Power) [已淘汰] 

    J2530A Token Ring-Parallel Port Adapter (North American Power) [已淘汰]

    This device allows the Keysight Advisor to be connected to the LAN via its parallel port in order to use the Keysight Advisor as a PC on a Token Ring LAN (not for testing LANs).

  • J2532A Ethernet-Parallel Port Adapter (International) [已淘汰] J2532A Ethernet-Parallel Port Adapter (International) [已淘汰] 

    J2532A Ethernet-Parallel Port Adapter (International) [已淘汰]

    This allows the Keysight Advisor to be used as a PC on a Ethernet LAN, by connecting the Keysight Advisor to the LAN via its parallel port (not for testing LANs).

  • J2533A Token Ring-Parallel Port Adapter (International) [已淘汰] J2533A Token Ring-Parallel Port Adapter (International) [已淘汰] 

    J2533A Token Ring-Parallel Port Adapter (International) [已淘汰]

    The Token ring-parallel port adapter (International) includes 4 and 16 Mbps interfaces (DB-9) plus software drivers.

  • J3308A Power Supply Upgrade Kit [已淘汰] J3308A Power Supply Upgrade Kit [已淘汰] 

    J3308A Power Supply Upgrade Kit [已淘汰]

    The upgrade for models Keysight J2301A, Keysight J2302A, Keysight J2522A or Keysight J2523A.