Keysight Oscilloscope Glossary
What Are the Trigger Types in Oscilloscopes?
Introduction
Did you know that the right trigger setting on an oscilloscope can mean the difference between capturing elusive glitches and spending hours in futile troubleshooting?
Just like how a camera's focus affects the clarity of a photograph, the trigger function dictates the effectiveness of your waveform analysis.
If you’re an electrical engineer or someone who works extensively with oscilloscopes, knowing your way around different trigger types isn’t just handy; it's essential.
Introduction to Triggering
Triggering stands as the cornerstone for obtaining reliable and accurate readings from an oscilloscope. It stabilizes a repeating waveform by providing a starting point for each wave cycle. Think of it as the conductor in an orchestra, setting the tempo and ensuring that everyone starts at the same point.
What Happens Without Proper Triggering?
- Jittery waveform: Lack of stability makes the analysis challenging.
- Missed details: Faulty trigger settings can skip over crucial glitches.
- Confusing display: Inconsistent trigger points can make it hard to interpret results.
Key Takeaway
Knowing the different trigger types in oscilloscopes helps you gather more accurate and meaningful data, regardless of the complexity of the signals. Choosing the right trigger can make all the difference in your measurements, so mastering this skill is crucial for anyone in electrical engineering and related fields.
The Importance of Selecting the Right Trigger Type
Choosing the right trigger type doesn't just make your oscilloscope more useful—it essentially broadens your analytical capabilities, opening up new avenues for problem-solving.
The right trigger type can help you handle a range of challenges. A well-set trigger can be helpful in various situations. Here are three examples.
Isolate Specific Conditions within a Signal
Imagine you are working with a complicated waveform that has many different frequencies or spikes. A well-set trigger allows you to hone in on a specific condition, such as a voltage spike, ignoring all other irrelevant parts of the waveform. This isolation can make it much easier to identify and diagnose issues.
Capture Non-Recurring Events Effectively
Some phenomena within electrical systems are transient—they appear for a brief moment and may not occur again for a long time.
A carefully selected trigger type, such as sequence triggering, can help you capture these fleeting events for analysis. This capability is invaluable when you're trying to track down rare glitches or anomalies in a system.
Make More Precise Measurements
The term "precision" in the world of oscilloscopes isn't just about showing a waveform clearly. It's about extracting meaningful data points and parameters from that waveform.
Here's how the right trigger setting contributes to more precise measurements:
- Noise reduction: Advanced triggers like holdoff triggering can filter out signal noise, allowing you to make cleaner, more accurate measurements.
- Time alignment: In applications requiring time-correlated signals from multiple channels, triggering ensures that all channels align perfectly in time, facilitating easier comparative analysis.
- Event characterization: Whether it’s the rise time, pulse width, or the amplitude of a signal, a precise trigger setting helps you measure these characteristics with greater accuracy. For instance, pulse-width triggering can be invaluable for measuring the width of pulses in a pulse-train to within fractions of a nanosecond.
- Resource optimization: When you can trust your measurements, you reduce the number of redundant tests and checks, ultimately saving both time and computational resources.
By understanding the nuances of various trigger types, you gain greater control over what you measure, how accurately you measure it, and under what conditions.
This heightened level of precision is not just a matter of quality—it often directly translates to cost and time efficiency in professional settings.
Basic Trigger Types
Understanding basic trigger types is fundamental to mastering oscilloscope usage. These triggers come as standard features in most oscilloscopes, and they offer a robust set of options for general-purpose measurements.
Edge Triggering
This is your everyday, workhorse trigger:
- Trigger point: Focuses on the rising or falling edge of a signal.
- Use case: Best for situations where you're interested in a particular event that happens as a waveform crosses a specific voltage level.
- Adjustments: The freedom to specify level and slope gives you control over where the oscilloscope starts drawing the waveform. You can adjust the trigger level to ignore low-level noise or to catch just the high-level events you're interested in.
Pulse Width Triggering
When waveforms get complex, pulse width triggering comes into play.
- Trigger point: Activates when a pulse width either meets or deviates from conditions you set.
- Use case: This is particularly useful in digital circuits where you need to isolate issues like jitter or timing errors.
- Adjustments: The ability to define the pulse width and polarity offers flexibility. You can set the trigger to capture pulses that are equal to, not equal to, less than, or greater than a specific width, giving you a powerful tool for isolating specific events.
Video Triggering
This is your specialized tool for video signal analysis.
- Trigger point: Targets specific lines or fields within a video frame.
- Use case: Engineers in broadcasting or anyone working on video signal repair will find this invaluable.
- Adjustments: With support for standard video formats like NTSC, PAL, and SECAM, this trigger type offers preset conditions that can make video signal analysis straightforward.
By mastering these basic but versatile trigger types, you set a strong foundation for effective and precise oscilloscope usage. Whether you're monitoring a simple sine wave or delving into the intricacies of a complex digital circuit, understanding how to leverage these triggers ensures that you can capture the data you need.
Advanced Trigger Types
While basic triggers cover a broad range of applications, advanced triggers come into play when you're dealing with more specialized or complex scenarios. These trigger types are not always available in entry-level oscilloscopes but are often found in high-end or specialized models.
Logic Triggering
Ideal for complex digital circuit diagnostics.
- Trigger point: Activates based on a set of logical conditions across multiple channels.
- Use case: Highly effective when you're monitoring digital signals that have multichannel interactions, like buses or digital logic circuits.
- Adjustments: You can set up rules based on Boolean logic conditions (AND, OR, XOR, etc.), allowing you to focus on specific combinations of signal states across different channels.
Sequence Triggering
For capturing events that happen in a particular order.
- Trigger point: Engages when a predefined series of conditions occur in a specific sequence.
- Use case: Especially useful when you're analyzing serial data streams or protocols where events must happen in a specific order for successful data transmission.
- Adjustments: You have the flexibility to define the sequence of conditions and the rules for each step, enabling you to isolate complex events for analysis.
Holdoff Triggering
Great for minimizing false triggers.
- Trigger point: Activates only after a set "holdoff" period has elapsed since the last trigger event.
- Use case: This is critical for signals with varying frequency or irregular events where a standard trigger might activate prematurely, capturing irrelevant data.
- Adjustments: You can set the duration of the holdoff period, which helps you ignore unwanted triggers.
- Additional consideration: Holdoff triggering is particularly helpful in avoiding “double-triggering” on unwanted events. For example, if you’re monitoring a pulse train with occasional glitches, setting the holdoff time just longer than the normal pulse width can make the scope ignore those glitches, allowing for cleaner data analysis.
Understanding and properly using these advanced trigger types enables you to extract meaningful data from highly complex or specialized waveforms.
Whether you're debugging a multi-layer digital circuit or capturing an elusive sequence of events in a communication protocol, advanced triggers offer the flexibility and specificity you need.
Select up to 3 instruments to compare
Tips for Effective Triggering
Even the most advanced oscilloscope won't serve its purpose if you're not adept at setting the right triggers. Here are some practical tips that can help you improve the effectiveness of your triggering setup.
1. Start with Basic Settings
If you're new to a particular application or unsure about the type of waveform you'll encounter, start with edge triggering. It's a versatile setting that can give you a basic but effective snapshot of your signal.
2. Analyze the Signal
Before venturing into more complex triggering options, spend some time analyzing your waveform. Use the oscilloscope's auto-set feature to get an initial view, and then consider what aspects of the signal you need to focus on. The better you understand your waveform, the more effectively you can set your triggers.
3. Adjust Sensitivity
The trigger sensitivity, often called "trigger level", can significantly impact your measurements. If set too high or too low, you risk either missing the event you want to capture or triggering on noise or other unwanted events. Take the time to fine-tune this setting.
4. Use External Trigger
Sometimes, the signal you want to analyze doesn't offer a convenient point to set an internal trigger. In these cases, you can often achieve more reliable triggering by using an external source.
This approach is especially useful in multi-device setups or when you need to synchronize your oscilloscope with another instrument.
- Synchronization: External triggering helps synchronize the oscilloscope with other test and measurement equipment. For example, you could use a signal generator's sync output as the external trigger to ensure that the scope starts capturing at a specific point in the generated waveform.
- Complex systems: In a system with multiple correlated signals, using an external trigger can help you align them in time for simultaneous observation and analysis.
- Special events: Some experiments or tests might use a specific event to start data capture, like a button press or another user action. An external trigger connected to this event ensures that your oscilloscope captures the data exactly when needed.
By incorporating these tips into your measurement practices, you can make more effective use of your oscilloscope, regardless of your level of expertise or the complexity of the signals you're working with.
Oscilloscope Trigger Types Reference Guide
| Trigger Type | Trigger Point | Use Case | Key Adjustments |
|---|---|---|---|
| Edge Triggering | Rising or falling edge of a signal | Analyze specific points in a regularly repeating waveform | Level and slope of the edge |
| Pulse Width Triggering | Matching pulse width conditions | Isolate issues like jitter in digital circuits | Define pulse width and polarity |
| Video Triggering | Specific lines or fields in video frame | Broadcast engineering, video signal repair | Standard video signal formats (NTSC, PAL, SECAM) |
| Logic Triggering | Logical conditions involving multiple channels | Multi-channel digital signals | Boolean logic conditions (AND, OR, XOR, etc.) |
| Sequence Triggering | Series of conditions in specific order | Capture complex sequences in serial data streams | Define the sequence and conditions for each step |
| Holdoff Triggering | After a defined "holdoff" period | Avoid false triggering in signals with varying frequency | Set the holdoff period |
Conclusion
Mastering the various trigger types available in modern oscilloscopes is akin to unlocking a toolkit full of specialized instruments. From the basic edge and pulse-width triggers to advanced logic and sequence triggers, each type serves a unique purpose and offers a different set of advantages.
Whether you're capturing simple waveforms, debugging intricate digital circuits, or analyzing specialized signals, understanding your trigger options enables you to extract more meaningful and precise data.
If you're looking to take your measurements to the next level, a premium oscilloscope with advanced triggering options is a worthy investment.
At the Keysight Used Equipment Store, you can find a range of high-quality used oscilloscopes, signal analyzers, function generators, and multimeters at competitive prices.
Opt for premium used equipment and elevate your testing capabilities. Don't compromise on quality or precision—Keysight offers the tools you need to excel.
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our Premium Used Oscilloscopes
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs