Keysight Oscilloscope Glossary
What Is an Analog-to-Digital Converter (ADC)?
Introduction
Imagine trying to watch a video on an old analog TV while living in a world of high-definition digital screens.
Just as our eyes crave the clarity of digital images, we love the ease and precision of the digital signals of modern electronic devices.
But how do they achieve this?
The answer lies in a critical component called an analog-to-digital converter (ADC), that bridges the analog and digital realms.
What is an ADC?
An analog-to-digital converter is a device that converts continuous analog signals into discrete digital numbers.
This conversion is essential because most modern electronics and computing systems operate using digital signals, which are easier to store, manipulate, and transmit than analog signals.
Key Takeaway
Analog-to-digital converters are essential for converting analog signals into digital data, impacting the performance of various electronic systems. Understanding their key parameters and types is crucial for selecting the right ADC for your applications.
How Does an ADC Work?
An ADC works by sampling the analog input signal at regular intervals and then converting the signal's amplitude into discrete values. This process involves two main steps:
- Sampling: The ADC takes periodic samples of the analog signal at a specific rate, known as the sampling rate or sampling frequency.
- Quantization: Each sampled value is then approximated to the nearest value within a finite set of discrete levels, producing a digital representation of the original analog signal.
Key Parameters of ADCs
To fully grasp how ADCs function, you need to understand their key parameters. These parameters determine the performance and suitability of an ADC for specific applications.
Resolution
The resolution of an ADC refers to the number of distinct values it can produce over the range of analog input. It is typically expressed in bits. For instance, an 8-bit = 256 levels; 14-bit = 16,384 levels (e.g., Keysight InfiniiVision HD3); 16-bit = 65,536 levels. Higher resolution results in more precise digital representation of the analog signal.
Sampling Rate
The sampling rate, or sampling frequency, is the number of samples taken per second. It is measured in samples per second (SPS) or Hertz (Hz). The sampling rate must be at least twice the highest frequency present in the analog signal to satisfy the Nyquist theorem and avoid aliasing.
Signal-to-Noise Ratio (SNR)
The signal-to-noise ratio (SNR) is a measure of how much desired signal is present compared to the background noise. Higher SNR indicates a clearer, more accurate representation of the original analog signal. SNR is usually expressed in decibels (dB).
Input Range
The input range is the range of analog signal levels that the ADC can convert. This range is defined by the minimum and maximum voltage levels that the ADC can handle.
Minimum and Maximum Voltage Levels
The minimum and maximum voltage levels define the boundaries within which the ADC operates effectively.
If the input signal falls below the minimum voltage or exceeds the maximum voltage, the ADC cannot accurately convert the signal. Ensuring that your analog signals stay within this range is crucial for accurate digital representation.
Dynamic Range
The dynamic range of an ADC is the ratio between the largest and smallest signals it can accurately convert. It is typically expressed in decibels (dB).
A higher dynamic range indicates that the ADC can handle a wider range of signal amplitudes, making it suitable for applications where the signal strength varies significantly.
Input Impedance
Input impedance refers to the resistance an ADC presents to the incoming signal. High input impedance ensures minimal loading on the signal source, preserving the integrity of the original analog signal.
Offset and Gain Error
- Offset error: This error occurs when there is a constant difference between the actual analog input and the converted digital output. It shifts the entire transfer function of the ADC.
- Gain error: This error is a proportional error that affects the slope of the ADC's transfer function. It causes the output to deviate from the ideal linear response, typically as a percentage of the full-scale output.
Understanding these key parameters will help you select the most appropriate ADC for your specific needs, ensuring optimal performance and accurate signal conversion.
Types of ADCs
Selecting the right type of ADC depends on your specific application needs, such as speed, resolution, and power consumption. Here are the main types of ADCs, each with its unique characteristics and use cases.
1. Successive Approximation Register (SAR) ADC
SAR ADCs are widely used due to their balance of speed, resolution, and power consumption. They work by using a binary search algorithm to converge on the input signal value. This type is ideal for applications requiring moderate speed and precision, such as data acquisition systems and instrumentation.
2. Sigma-Delta (ΣΔ) ADC
Sigma-Delta ADCs are known for their high resolution and excellent noise performance. They oversample the input signal and use digital filtering to achieve high accuracy. These are well-suited for audio applications, precision measurement, and instrumentation where noise performance is critical.
3. Flash ADC
Flash ADCs are the fastest type, capable of converting signals in a single step. They use a parallel array of comparators to convert the input signal, making them suitable for high-speed applications but at the cost of higher power consumption and lower resolution. This type is commonly used in digital oscilloscopes, radar systems, and high-speed data acquisition.
4. Dual Slope ADC
Dual slope ADCs are known for their high accuracy and noise rejection. They integrate the input signal over a period, then measure the result, making them suitable for applications where precision is more important than speed. This type is often used in digital multimeters and other precision measurement instruments.
Comparison of ADC Types
| Type | Resolution | Speed | Power Consumption | Power Consumption | Typical Applications |
|---|---|---|---|---|---|
| SAR ADC | Medium to High | Medium | Low | Moderate | General-purpose, data acquisition |
| Sigma-Delta (ΣΔ) ADC | High | Low to Medium | Medium | High | Audio, instrumentation |
| Flash ADC | Low to Medium | High | High | Low | High-speed data acquisition, radar |
| Dual Slope ADC | High | Low | Low | High | Precision measurement, multimeters |
Medium to High
Medium
Low
Moderate
General-purpose, data acquisition
High
Low to Medium
Medium
High
Audio, instrumentation
Low to Medium
High
High
Low
High-speed data acquisition, radar
High
Low
Low
High
Precision measurement, multimeters
Applications of ADCs in Testing Equipment
ADCs play a vital role in the performance of oscilloscopes and other testing equipment. These devices rely on ADCs to convert analog signals from probes and sensors into digital data that can be processed, displayed, and analyzed.
Oscilloscopes
Oscilloscopes use ADCs to sample electrical signals at high speeds. The resolution and sampling rate of the ADC determines the oscilloscope's ability to accurately capture and display waveforms. High-speed ADCs with high resolution are essential for observing fast transients and subtle signal variations in electronic circuits.
Signal Processing in Oscilloscopes
- Signal input: The oscilloscope receives the electrical signal through its input terminal, connected via a probe to the circuit under test.
- Amplification and attenuation: A pre-amplifier boosts the incoming signal, and the vertical controls adjust the level of amplification. High-voltage signals may be attenuated to bring them within a measurable range.
- Sampling: The horizontal system of the oscilloscope digitizes the input signal at a given sample rate. These samples are stored in memory, forming a waveform record. The sample rate needs to be high enough to accurately reconstruct the waveform, at least 2 times the oscilloscope's bandwidth to avoid aliasing.
- Digital conversion: The ADC converts the analog signal into digital data that the oscilloscope can process and display. The resolution of the ADC affects the vertical precision, while the sampling rate affects the horizontal time resolution.
- Display and analysis: Modern digital oscilloscopes use LCD or LED screens to display the waveform, allowing for advanced features such as zoom, pan, and mathematical operations on the waveform. Advanced triggering options, like edge, pulse, and logic triggering, help in capturing and analyzing specific signal events.
What's the Difference Between an 8-Bit and a 14-Bit Oscilloscope?
An 8-bit ADC splits the input range into 256 vertical levels. A 14-bit ADC, like the one in the Keysight InfiniiVision HD3 Series, splits it into 16,384 vertical levels, or 64 times finer resolution. That is more than a spec-sheet detail. It can be the difference between seeing millivolt ripple on a power rail and seeing a trace that looks flat. The HD3 pairs its 14-bit ADC with a 50 µVrms noise floor, so small signals are easier to see instead of getting lost in quantization steps. If you measure power integrity, sensor outputs, or anything small riding on something big, ADC resolution can be just as important as bandwidth when choosing an oscilloscope.
Digital Multimeters
Digital multimeters use ADCs to measure voltage, current, and resistance with high accuracy. Dual slope ADCs are commonly used due to their precision and noise rejection capabilities. The ADC's performance directly impacts measurement accuracy and reliability.
Spectrum Analyzers
Spectrum analyzers rely on ADCs to convert input signals into digital data for frequency domain analysis.
The ADC's sampling rate and resolution affect the analyzer's ability to detect and measure signal components across a wide frequency range. High-performance ADCs enable spectrum analyzers to provide detailed insights into signal behavior and interference.
By incorporating high-quality ADCs, oscilloscopes and other testing equipment can achieve greater accuracy, reliability, and functionality, making them indispensable tools for engineers and technicians in various fields.
비교할 최대 3개 기기를 선택하세요
Conclusion
Analog-to-digital converters are crucial components in electronic systems, converting analog signals into digital data for accurate processing and analysis.
Key parameters like resolution, sampling rate, signal-to-noise ratio, and input range determine their effectiveness.
Various ADC types, including SAR, Sigma-Delta, Flash, and Dual Slope, cater to different application needs, from general data acquisition to high-speed signal processing.
For high-quality and reliable testing equipment, explore premium used oscilloscopes, spectrum analyzers, function generators, and multimeters at the Keysight Used Equipment Store.
We offer the best instruments at affordable prices, ensuring you get the performance you need. Visit the Keysight Used Equipment Store to find the perfect tools for your next project.
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our Premium Used Oscilloscopes.
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs