Keysight Oscilloscope Glossary
What are Automotive Oscilloscopes?
Introduction
An automotive oscilloscope is a specialized diagnostic tool designed specifically for automotive applications. It lets you capture, display, and analyze electrical signals within a vehicle's complex electrical system.
Automotive scopes are critical for automotive diagnostics, especially with the increasing complexity of modern vehicle systems, including electric vehicles.
Key Takeaway
An automotive oscilloscope is a specialized tool that analyzes electrical signals and checks various electrical parts on vehicles.
The Growing Importance of Automotive Oscilloscopes in the Automotive Industry
As vehicles increasingly rely on electronics and sophisticated control systems, the need for accurate and efficient diagnostic tools like automotive oscilloscopes has become more important than ever.
With the massive increase of electric vehicles and advanced driver-assistance systems (ADAS), the complexity of automotive electrical systems will only continue to increase.
Automotive oscilloscopes provide you and other technicians with a versatile and powerful tool for diagnosing and troubleshooting these complex systems, ensuring modern vehicles' safe and reliable operation.
By understanding the key specifications, probe technologies, and advanced features of automotive oscilloscopes, you can make the best decision about the tools you need to tackle the diagnostic challenges of today and the future.
Why Not Use a Standard Oscilloscope?
While a standard oscilloscope can be used for some automotive measurements, they often lack the specific features, probes, and capabilities to make efficient and accurate automotive diagnostics.
Automotive oscilloscopes can handle the unique challenges of automotive industry applications, such as intermittent faults, a wide range of voltage levels, and the need for deep memory and high sample rates.
How an Automotive Oscilloscope Works
An automotive oscilloscope converts an electrical signal, such as voltage or current, into a visual waveform that is then analyzed on the oscilloscope screen. This allows you to see the behavior of electronic components and systems within a vehicle and identify any issues or faults.
The automotive scope can also store and compare waveforms to identify intermittent faults and determine if the problem is with a specific component or the vehicle's electrical system as a whole.
Benefits of Using an Automotive Oscilloscope
There are many benefits to using an automotive oscilloscope.
- Enhanced diagnostics. Automotive scopes offer automatic measurement functions that simplify the analysis of complex signals, helping you identify issues quickly and accurately.
- Detection of intermittent faults. The deep memory and high sampling rate of automotive oscilloscopes allow you to capture and analyze intermittent faults.
- Wide range of applications. Automotive oscilloscopes are used for a variety of automotive applications, from analyzing sensor data to testing the operation of electric vehicle components.
Automotive Oscilloscope Applications
Let's explore some of their common applications to further illustrate the importance and versatility of automotive oscilloscopes.
- Accurate analysis of engine and transmission control systems. Automotive oscilloscopes can analyze signals from various sensors, such as crankshaft and camshaft position sensors, throttle position sensors, and transmission speed sensors. This analysis enables you to diagnose issues related to engine performance, fuel efficiency, and emission control systems.
- Ignition systems. By monitoring ignition coil primary and secondary voltage waveforms, automotive oscilloscopes can help diagnose issues related to misfires, poor engine performance, and excessive emissions.
- Fuel injection systems. Automotive oscilloscopes can analyze fuel injector voltage and current waveforms, helping to diagnose issues like poor fuel atomization, leaking injectors, and uneven fuel distribution.
- Electric vehicle systems. With the growing popularity of electric vehicles, automotive oscilloscopes are increasingly being used to diagnose issues related to battery management systems, electric motor control, and charging systems.
- Advanced driver-assistance systems (ADAS). As vehicles incorporate more advanced safety features, automotive oscilloscopes can diagnose issues with sensors, cameras, and control systems in ADAS, ensuring these systems function correctly and safely.
Key Specifications To Look For
When selecting an automotive oscilloscope, consider the following specifications.
- MHz bandwidth. A higher bandwidth allows for capturing and analyzing higher-frequency signals, which is essential for modern vehicles with high-speed communication systems.
- Input channels. The number of input channels should be sufficient for your specific automotive applications.
- Memory depth. A deeper memory lets you capture and analyze signals for longer periods, which helps detect intermittent faults.
- Sample rate. A higher sample rate ensures an accurate electrical signal representation, which is crucial for accurate automotive diagnostics.
- Handheld or benchtop. Depending on your workspace and mobility requirements, you can choose between a handheld oscilloscope or a benchtop model.
What Probes Should You Use?
Selecting the appropriate probes for your automotive oscilloscope is critical for safe and accurate measurements. Probe technologies suitable for automotive applications include the following:
- High-voltage probes. These probes can handle high voltage levels in certain automotive systems, such as ignition and electric vehicles.
- Pressure transducer. A pressure transducer converts pressure measurements into electrical signals that can be analyzed by the oscilloscope, making them useful for monitoring fuel pressure, intake manifold pressure, and more.
- Current probes. These probes measure current flow through a circuit and help monitor starter motor current, alternator output, and other high-current applications.
By utilizing automotive probes, you can efficiently and accurately diagnose a wide range of issues in modern vehicles, improving the quality and reliability of automotive diagnostics in the industry.
Advanced Features in Automotive Oscilloscopes
In addition to the basic specifications and probe selection, several advanced features can further enhance the capabilities of an automotive oscilloscope.
- Predefined automotive tests. Some oscilloscopes come with built-in automotive tests, such as CAN bus decoding, LIN bus analysis, and ignition waveform analysis, which can save time and improve diagnostic accuracy.
- Advanced triggering options. Advanced triggering options, like pulse width and window triggers, can help capture specific events or electrical signal anomalies, making diagnosing complex issues easier.
- Waveform math and analysis functions. These functions enable the oscilloscope to perform real-time calculations and analysis on captured waveforms, including filtering, integration, differentiation, and more.
- Connectivity and data storage options. Look for oscilloscopes with USB, Ethernet, or wireless connectivity options for easy data transfer and storage and integration with other diagnostic tools and software.
Keysight Oscilloscopes
Buying a used oscilloscope is the best way to save money without sacrificing quality. You can save up to 90% when purchasing from the Keysight Used Equipment Store!
We offer a wide range of high-quality, premium refurbished oscilloscopes backed by a 1-year warranty. You can be confident you are choosing a quality oscilloscope supported by a trusted manufacturer.
Check out our premium Used Equipment page to choose a premium refurbished oscilloscope with some of the highest standards and specifications in the industry.
비교할 최대 3개 기기를 선택하세요
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our Premium Used Oscilloscopes.
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs