Joomla component Questions SQL Injection

Strike ID:
E18-5na91
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
6
Year:
2018

Description

This strike exploits a SQL injection vulnerability in the Questions component for Joomla!. The vulnerability is due to the improper sanitization of requests sent to the application. An attacker could exploit this vulnerability by sending specifically crafted packets, potentially resulting in the execution of SQL commands which may lead to information disclosure.

CVE