WordPress Plugin Anti-Malware and Brute-Force Firewall Local File inclusion

Strike ID:
E19-0zyy1
CVSS:
5.0 (AV:N/AC:L/Au:N/C:P/I:N/A:N)
False Positive:
f
Variants:
1
Year:
2019

Description

This strike exploits a local file inclusion vulnerability in WordPress Plugin Anti-Malware and Brute-Force Firewall 4.18.63. The vulnerability is due to improper sanitization of the base64 encoded GOTMLS_scan parameter. By successfully exploiting this vulnerability, an authenticated attacker could retrieve arbitrary files from the target server.