VMware Cloud Director Expression Language Authenticated Java template injection

Strike ID:
E20-11h01
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:L/UI:N/S:U/C:H/I:H/A:H
False Positive:
t
Variants:
4
Year:
2020

Description

A command injection vulnerability exists in VMware Cloud Director. The vulnerability is due to the lack of sanitization while parsing input passed to 'hostname' parameter within the SMPT configuration form. An authenticated attacker can exploit this vulnerability by crafting a malicious HTTP PUT request. Successful exploitation results in full control of the cloud director platform.

CVE

References