E18-5op31
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
t
Variants:
1
Year:
2018
Description
This strike exploits a remote code execution existing in the WordPress GDPR Compliance plugin.
The vulnerability resides in the lack of requests authorization when performing the AJAX 'wpgdprc_process_action' call as a unauthenticated user, resulting in alteration of database entries.
An attacker is thus able to add a privileged user to a WordPress platform and subsequently execute PHP code as the user under which the HTTP server runs.