Dasan GPON Home Router GponForm dest_host OS Injection

Strike ID:
E18-5i0y1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018

Description

An arbitrary file overwrite vulnerability has been identified in Dasan GPON Home Router. The vulnerability is caused by the lack of proper input sanitisation of 'dest_host' parameter within the 'GponForm'. The vulnerability can be exploited by sending a specially-crafted POST request, allowing the attacker to execute arbitrary commands on the device with root privileges.

CVE

References