HPE Operations Orchestration central-remoting Remote Code Execution

Strike ID:
E17-0i7m1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2017

Description

This strike exploits a remote code execution vulnerability in Hewlett Packard Operations Orchestration. The vulnerability is due to insecure deserialization of user input data sent through HTTP. A remote, unauthenticated attacker can run arbitrary commands on the targeted system under the context of the user running the web application.

CVE

References

Metasploit

Zdi

Bid