Windows mshtml Engine Remote Code Execution

Strike ID:
E19-0r4d1
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2019

Description

This strike exploits a vulnerability in the Microsoft mshtml Engine. The vulnerability is due to improper filtering of the "edit" parameter. An attacker could exploit this vulnerability by enticing the victim to click a malicious link and download the malicious html file. Successful exploitation may lead to remote code execution on the client.

CVE

Bid