Windows VBScript Engine Use After Free

Strike ID:
E18-0pam1
CVSS:
7.5 CVSS:3.0/AV:N/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018

Description

This strike exploits a vulnerability in Microsoft VBScript Engine. Specifically the vulnerability fakes and overrides the array object to perform arbitrary address reading and writing. In the end, it releases code to execute after constructing an object. An attacker who successfully exploited the vulnerability could gain the same user rights as the current user.

CVE

References