D-Link DSR-250N Denial of Service

Strike ID:
D20-a4p31
CVSS:
7.5 CVSS:3.1/AV:N/AC:L/PR:N/UI:N/S:U/C:N/I:N/A:H
False Positive:
f
Variants:
1
Year:
2020

Description

This strike exploits a vulnerability inside D-Link Wireless N Unified Service Routers (DSR-250N) 3.12 that can cause a denial of service attack. The device which allows unauthenticated attackers in the same local network to execute a CGI script which reboots the device. The attack can be triggered without authentication.

CVE