BenchVue Software

Lab Management Client App

This bundle is part of PathWave BenchVue Software

Installs on: Computer


Key Features

  • The BenchVue Lab - Client software application (Client App) is designed for a lab setup environment where the instruments from each bench are connected and controlled by a dedicated PC. The Client App is installed on each of the test bench PC.
  • The test bench PC connects all the instruments on a test bench via GPIB/USB/LAN/RS-232 and communicates to the Manager App in the same network. The Client App can support up to a maximum of six instruments per bench.
  • The Client App supports over five hundred Keysight test instruments as well as non-Keysight test instruments that are compliant with the VISA connection protocol.
  • The Client App includes a lab configuration feature that enables students to configure instruments on their respective bench.

This Bundle Includes

  • BenchVue Lab Management Client App

 


Prerequisite Software

In order to use this bundle, you must also have the following:

System Requirements

Instrument Compatibility

This Bundle Is Part of…

PathWave BenchVue Software — Software apps for easy instrument control and simplified automation.


Learn more: PathWave BenchVue Software

Select a Configuration