|
What Do I Have to Do to Run a Test Fixture That Was Developed for Bank I on a Bank II System?
Question:
What do I have to do to run a test fixture that was developed for
bank I on a bank II system?
Answer:
(Date: Apr 97: Version: B.02.XX) To run a bank I fixture on a bank
II system (run a "left-handed" fixture on a "right-handed"
testhead), you need to run the fix_flip and wire_flip contributed
utilities. Fix_flip maps the fixture file from one bank to another,
wire_flip maps the wirelist from one bank to another. These utilities
are located in the /usr/hp3070/contrib/bin directory along with
an instruction document in /usr/hp3070/contrib/doc/flip.doc
A few things you need to keep in mind after running the utilities
are:
-
Make sure the fixture id, fixture enable and safety disable
pins are wired correctly in the front module (1 or 3). Fix_flip
will make these changes to the fixture.flip file automatically
and will write messages to the screen about which pin wires
the user needs to change.
-
Edit the board file to say bank1 instead of bank2 or vice-versa.
-
Edit the board "config" file to include the new
modules that are now being used, and comment out the ones that
are not.
-
Make sure power supply numbers match up correctly in the "config"
file.
-
Edit the vacuum well statement in testplan.
-
Remember, the fixture will now be placed on the opposite bank
of the testhead and will be rotated by 180 degrees.
|