Article Reprints
Keysight Technologies
Testing a Network Communication PCBA from Prototype to Manufacturing
Article Reprint
Testing a Network Communication PCBA from Prototype to Manufacturing
Early implementation of BST can cut test costs and time.
The Network Communications (netcomm) printed circuit board assembly is one the largest boards in terms of size, number of nodes/nets and components. It also has the most advanced technology in terms of speed and complexity. The quality of a product and its suc-cess depends on deploying an effective manufacturing test strategy to catch structural defects and prevent bad boards from flowing down to the functional station, box build or, at worst, into customers’ hands.
The manufacturing process of netcomm PCBAs faces many test challenges, mainly due to the loss of test access with the prevalence of the following technologies:
Boundary scan is an important strategy to recover test coverage for netcomm boards during manufacturing test. Below are the following IEEE standards and bound-ary scan test system features that enable test engineers to recover manufacturing test:
1. IEEE Std. 1149.1. IEEE Std. 1149.1, the IEEE Standard for Test Access Port and Boundary-Scan Architecture, is the foundation of the boundary scan standard that enables testing of the intercon-nect between two or more boundary scan devices. Test features enabled on 1149.1 are:
2. IEEE Std 1149.6. IEEE Standard for boundary scan testing of advanced digital networks cov-ers the differential signal (LVDS). The following tests are generated using 1149.6 standard:
Boundary scan is cost-effective because it can be integrated into every stage of the PCBA manufacturing test-ing to recover coverage for those nodes/nets that have no test access, while at the same time reducing manufacturing test cost.
Now let’s look at how a typical netcomm board is built, as it will give us a good idea on the test requirements and potential solutions:
3. Prototype build. This is the ini-tial step where the design center or R&D team builds the board to ver-ify software and hardware design.
Boundary scan test program development can be developed at the early stage of board develop-ment where only limited infor-mation is available, such as the netlist, bill of materials (BoM) and boundary scan description language (BSDL) of boundary scan devic-es. The test engineer will be able to feed back to the board design engineer any necessary changes to the board before fabrication that will enable BST and maximize test coverage during manufacturing test-ing. The following boundary scan design for test can be captured during program development:
4. New product introduction. This step involves a lot of work toward testing boards and verifying their manufacturability. Boards that are built will then be shipped to various sites of the company, or to custom-er sites and government bodies for certification and testing.
During the NPI stage, the in-cir-cuit test (ICT) fixture will be fabricated to ready it for production testing. Integration and implementation of boundary scan from prototype to ICT will significantly reduce cost on test program development, and debugging of boundary scan tests is performed during the prototype stage. Also dur-ing the prototype stage, boundary scan issues can be found early and resolved before progressing onto the building of ICT fixture at NPI.
Typical netcomm nodes/nets can range from 6,000 to more than 10,000 per board. A PCBA designed for BST will be able to test at least 40% of these nodes, thus reducing ICT fixture and system requirements.
An obvious benefit is the lower cost of ICT fixtures. Nodes/nets tested identified and verified during prototyp-ing by boundary scan can be removed from the ICT fixture. This will trans-late to significant cost-reduction for fabrication of the ICT fixture.
What are you looking for?