AGILENT 53200A SERIES 350 MHz UNIVERSAL and RF FREQUENCY COUNTERS

EXAMPLE PROGRAMS

 

 

You have a royalty-free right to use, modify, reproduce and distribute the Example Program Files (and/or any modified version) in any way you find useful, provided that you agree that Agilent has no warranty, obligations, or liability for any example program.

 

Agilent Technologies provides programming examples for illustration only.  The examples assume that you are familiar with the development environment and its associated tools and debug procedures. Agilent Support Engineers can help explain the functionality of Agilent software components and associated commands, but they will not modify the examples to provide added functionality or construct procedures to meet your specific needs.

 

 

Organization

 

The example programs were developed using the following programming languages:

 

Microsoft Visual Basic 6.0

Microsoft C# (Visual Studio 2008)

 

Examples are provided for:

Basic Measurement

Fastest Measurement

Multi Set Measurement

Reading Threshold Measurement

Statistics Functions

Status Register Monitor

Time Stamp Measurement

VISA Com Time Interval Measurement

 

 

Purpose

 

The example programs are provided solely for the purpose of illustrating basic counter functionality and the SCPI (Standard Commands for Programmable Instruments) commands used to perform the measurements. They are not intended to demonstrate the environment or IO. 

 

Microsoft® and Visual BASIC® are U.S. registered trademarks of Microsoft Corporation.

 

Copyright © 2010 Agilent Technologies Inc. All rights reserved.