Agilent E4438C ESG, E8267C PSG and E8267D PSG
Option 420
Signal Studio for Pulse Building
Software 1.0.34.0 through 1.0.51.0 Release Descriptions

NOTE:  Features depend on installed hardware and software options in the signal generator.


Software 1.0.51.0 Released June 30, 2005

Software 1.0.50.0 Released October 29, 2004

Software 1.0.49.0 Released March 17, 2004

Software 1.0.39.0 Released July 7, 2003

Software 1.0.38.0 Released June 26, 2003

Software 1.0.34.0 Released December 4, 2002

Related Information

Technical Overview
Installation Instructions

Download Evaluation Copy

Upgrading Firmware

Contact Us / Provide Feedback
 


Software 1.0.51.0

Software version 1.0.51.0 is a revised version of E4438C, E8267C and E8267D Option 420 Signal Studio for Pulse Building.

Software 1.0.51.0 Bug Fixes

        Download and play now works for the following firmware revisions:

o       E8267D with firmware revision C.04.17 or higher

o       E8267C with firmware revision C.03.80 or higher

o       E4438C with firmware revision C.04.10 or higher

        API now works correctly.

Back to top of page


Software 1.0.50.0

Software version 1.0.50.0 is a revised version of E4438C, E8267C and E8267D Option 420 Signal Studio for Pulse Building.

Software 1.0.50.0 Enhancements

 

Back to top of page


Software 1.0.49.0

Software version 1.0.49.0 is a revised version of E4438C and E8267C Option 420 Signal Studio for Pulse Building.

Software 1.0.49.0 Enhancements

Software 1.0.49.0 Issues Resolved

Updated the help file.

Software 1.0.49.0 Hardware and Firmware Compatibility

Note

Supported operating systems:

  • Windows XP Professional (Service Pack 1 or later)
  • Windows 2000 (Service Pack 3 or later)
  • Windows NT 4.0 (Service Pack 6a or later)

Microsoft .NET framework (Service Pack 2 or later) must also be installed. See the Signal Studio Installation Guide for details.

Signal Studio software 1.0.49.0 is compatible with the following hardware and firmware options of the E4438C ESG vector signal generator:

Signal Studio Software

E4438C ESG Vector
Signal Generator Hardware Options

E4438C ESG Vector
Signal Generator Firmware

1.0.49.0

Works with all hardware options.

Firmware C.03.62 and above

Signal Studio software 1.0.49.0 is compatible with the following hardware and firmware options of the E8267C PSG vector signal generator:

 Signal Studio Software

E8267C PSG Vector
Signal Generator Hardware Options

E8267C PSG Vector
Signal Generator Firmware

1.0.49.0

Works with all hardware options.

Firmware C.03.05 and above

To upload encrypted waveform files from the signal generator, firmware version C.03.31 or later is required.

 

Back to top of page


Software 1.0.39.0

Software version 1.0.39.0 is a revised version of E8267C Option 420 Signal Studio for Pulse Building.

Software 1.0.39.0 Issues Resolved

 

 Back to top of page


Software 1.0.38.0

Software version 1.0.38.0 is a revised version of E8267C Option 420 Signal Studio for Pulse Building.

Software 1.0.38.0 Enhancements

        Added support for Option 602 internal baseband generator with digital bus capability.

        Added the ability to upload encrypted waveforms from the signal generator. This gives the user the ability to transfer a waveform from the signal generator to a computer and then download this waveform to a different signal generator. Requires firmware C.03.31 or later.

 

NOTE: If the waveform was created with an optional signal creation application (i.e. Signal Studio or a waveform created within the PSG), the signal generator is required to have the license key (alpha-numeric code) for that particular option installed before playback of that waveform is allowed.

 Software 1.0.38.0 Issues Resolved

Software 1.0.38.0 Hardware and Firmware Compatibility

Note

Supported operating systems:

  • Windows XP Professional (Service Pack 1 or later)
  • Windows 2000 (Service Pack 3 or later)
  • Windows NT 4.0 (Service Pack 6a or later)

Microsoft .NET framework (Service Pack 2 or later) must also be installed. See the Signal Studio Installation Guide for details.

Signal Studio software 1.0.38.0 is compatible with the following hardware and firmware options of the E8267C PSG vector signal generator:

Signal Studio Software

E8267C PSG Vector
Signal Generator Hardware Options

E8267C PSG Vector
Signal Generator Firmware

1.0.38.0

Works with all hardware options.

Firmware C.03.05 and above

To upload encrypted waveform files from the signal generator, firmware version C.03.31 or later is required.

 Back to top of page


Software 1.0.34.0

Software version 1.0.34.0 is the initial version of E8267C Option 420 Signal Studio for Pulse Building and is used to simplify the creation of complex, single-emitter, radar test patterns with custom pulse shaping and pulse compression.

The Pulse Building personality includes the ability to:

Software 1.0.34.0 Hardware and Firmware Compatibility

Note

Supported operating systems:

  • Windows XP Professional (Service Pack 1 or later)
  • Windows 2000 (Service Pack 3 or later)
  • Windows NT 4.0 (Service Pack 6a or later)

Microsoft .NET framework (Service Pack 2 or later) must also be installed. See the Signal Studio Installation Guide for details.

Signal Studio software 1.0.34.0 is compatible with the following hardware and firmware options of the E8267C PSG vector signal generator:

Signal Studio Software

E8267C PSG Vector
Signal Generator Hardware Options

E8267C PSG Vector
Signal Generator Firmware

1.0.34.0

Works with all hardware options.

Firmware C.03.05 and above

 

Back to top of page


Copyright 2003-2005 Agilent Technologies, Inc. All rights reserved.
Other product and company names herein may be the trademarks of their respective owners.