Column Control DTX

EMI Troubleshooting: The Need for Close Field Probes

白皮書

Close field electromagnetic interference (EMI) tests are a valuable tool in electromagnetic compatibility (EMC) radiated emission pre-compliance testing. Close field testing is performed at short distances. Far Field testing is performed at distances between 3 to 10 meters at test facilities using EMI receivers and antennas. The nature of the electromagnetic field is determined by the device under test (DUT) and the distance of the receivers and antennas from the DUT. A far field radiated emission measurement accurately determines if the DUT is compliant to related EMC/EMI standards.

 

However, far field testing has limitations. It cannot identify the source of emissions. Radiated emissions may come from a USB port, a LAN port, the seam of a shield, a cable, or even a power cord. Close field testing is the only way to locate the exact source of the emission and is typically performed using a signal analyzer and close field probe.

×

請銷售人員與我聯絡。

*Indicates required field

您希望以何種方式取得相關資訊? *必填欄位
Preferred method of communication? 變更email?
Preferred method of communication?

請點擊按鈕後,提供給是德科技您的個人資料。您可以從 Keysight隱私聲明 中,閱讀到我們如何使用這些資料的訊息,謝謝。

感謝您!

A sales representative will contact you soon.

Column Control DTX