Column Control DTX

Troubleshooting VFDs with Low Pass Filter

應用說明

Today, three-phase induction motors are the most important workhorses in industry and commercial facilities. An AC induction motor is commonly used as a constant-speed drive when fed from a voltage source of fixed frequency. Unfortunately, running a motor at maximum speed, regardless of the varying demands of production, means a great deal of electric power is wasted. In many motor applications, energy use can be reduced considerably if the speed of the motor varies in response to the changing process conditions. With the advent of solid state electronics, variable speed drives can regulate the speed of a three-phase AC electric motor by converting three-phase AC line voltage to a quasi-sinusoidal pulse width modulated (PWM) waveform in which the frequency and voltage level can be varied.

×

請銷售人員與我聯絡。

*Indicates required field

您希望以何種方式取得相關資訊? *必填欄位
Preferred method of communication? 變更email?
Preferred method of communication?

請點擊按鈕後,提供給是德科技您的個人資料。您可以從 Keysight隱私聲明 中,閱讀到我們如何使用這些資料的訊息,謝謝。

感謝您!

A sales representative will contact you soon.

Column Control DTX