Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

T1212S Bluetooth® Protocol Conformance Test System

Статус продукта: Производство прекращено | Поддерживается
Этот продукт больше не поставляется

Для данного продукта вариантов замены не найдено.

Ключевые возможности и технические характеристики

  • Officially validated by the Bluetooth SIG for protocol qualification.
  • Supports testing of V1.2, V2.0+EDR, V2.1+EDR, 3.0, 4.0 and low energy technologies in just one single platform.
  • Supports testing of LL and HCI for Bluetooth low energy test specifications.
  • Supports 3.0 and 4.0 Protocol test cases for BB, LM, HCI and GAP layers.
  • Based on the official TTCN BT SIG test cases.
  • Manual/Automatic test cases selection.
  • Verdict handling and test log analysis.
  • Supports test cases execution form different layers within the same test campaign.

Описание

T1212S BITE Bluetooth® Protocol Conformance Tester is an integrated test tool that performs automatically V1.2, V2.0+EDR, V2.1+EDR, 3.0, 4.0 and Bluetooth low energy protocol test cases required for the qualification of Bluetooth devices. BITE T1212S is the only test platform officially validated by the Bluetooth SIG for Protocol qualification of Bluetooth devices.

T1212S integrates the Test Manager software application to control all the testing workflow, from the connection of the device under test to the tester to the final generation of the test report, including data collection, test plan generation, test execution and results analysis.