Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

Nenhum substituto foi encontrado para esse produto.

Principais recursos e especificações

Option 1EM moves the following front panel connectors to the rear panel:

  • RF Output
  • LF Output
  • Ext1 AND Ext2 Inputs
  • Gate/Pulse/Trigger Input
  • ALC Input
  • Sync Out
  • Video Out

Descrição

Convenient connector placement for use in rackmount environments

The E8663B equipped with Option 1EM provides rear panel connectors only. With this option, all front panel connectors are moved to the rear panel of the instrument.

Typical application

Rear-panel connectors are recommended to simplify cable management when installing and using the E8663B in rackmount test environments such as manufacturing and system verification. Rear-panel connectors significantly simplify installation and maintenance and enable orderly cable management.