Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

E2698A Ethernet Mask Testing Option

Status do Produto: Obsoleto | Veja opções de Serviço
Este produto não se encontra disponível

Esse produto foi substituído por um novo:

Descrição

This product will be discontinued on November 1, 2005. Please consider its replacement, the new Keysight N5392A, Ethernet Electrical Performance Validation and Compliance Software

The E2698A will be discontinued on November 1, 2005. N5392A Ethernet Electrical Performance Validation and Compliance Software

The E2698A Ethernet Masks provide mask templates for 1000BaseTX, 100BaseT and 10BaseT. These masks are supported for both the Infiniium 54850-series and Infiniium 54830-series of oscilloscopes with version A.03.10 system software or later installed (Windows® XP Pro), and provide pass/fail testing for Ethernet signals.

Masks provided:

1000BaseTX: six masks (points A, B, C, D, F and H as specified in paragraph 40.6.1.1.2 and figure 40-19 of IEEE 802.3-2002 specification). The masks assume that the user has properly connected a differential probe from channel 1 of the oscilloscope to one pair of the transmitter under test (as in 802.3-2002 paragraph 40.6.1.1.3) and that Test Mode 1 (802.3-2002 paragraph 40.6.1.1.2) is enabled.

You also receive two mask templates for 100BaseT and four mask templates for 10BaseT.