Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

Configuração Típica  

Configuração Típica

N6466A MOST Compliance Application for Infiniium scopes

  • EDEL-ONLY-01 License certificate delivery - email only

Configure

Preço para o: Brasil

* Os preços não incluem impostos ou taxas, os quais deverão ser considerados na oportunidade em que emitida a cotação formal, conforme determinação das autoridades governamentais competentes. Os preços mostrados são os preços de varejo sugeridos pelo fabricante (MSRP). Os preços apresentados não incluem impostos.

Principais recursos e especificações

Standards Supported:

  • The N6466A MOST compliance application supports MOST50 and MOST150 (cPhy and oPhy) technology standards.
  • The application automates 100% compliance test coverage for all tests.
  • Testing can be done at the oscilloscope or remotely using programmatic commands. Programmability allows, for example, testing over an extended period of time in an environmental chamber.

Automation:

  • Automated setups ensure result repeatability and enable test engineers to run the application without being an expert on MOST50 and MOST150 testing procedures.
  • Test setup wizard guides user through test selection, configuration, connection, execution and results reporting.
  • Oscilloscope setup is automatically configured for each test, and measurement connection setups are displayed.
  • Test results report documents test configuration, measurements made, pass/fail status, margin analysis and waveforms.

Requirements:

  • The N6466A MOST compliance application embeds jitter and SDA functionality needed for MOST testing, eliminating the need to purchase additional apps.
  • MOST50 compliance testing requires Infiniium oscilloscopes with 500 MHz or greater bandwidth.
  • MOST150 compliance testing requires Infiniium oscilloscopes with 1 GHz or greater bandwidth.
  • While the MOST150 cPhy compliance tests use a differential probe (1.5 GHz or higher), MOST150 oPhy tests additionally require an optical-to-electrical converter probe.

Extensibility:

  • The application can be ordered as a fixed license for a specific oscilloscope. The application can also be ordered as a server-based floating license using N5435A option 068, allowing the application license to move between multiple oscilloscopes.
  • Use the N5467A user-defined application tool (www.keysight.com/find/uda) to add additional custom tests beyond the MOST technology standards.
  • Keysight’s 81160A pulse/function generator can be used as the source for MOST150 stress pattern testing.

Descrição

The N6466A MOST compliance application for Infiniium oscilloscopes simplifies and accelerates MOST technology standards testing.