Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

Beam Directing and Reflecting Optics

Beam directing and reflecting optics simply reflect, bend or translate the beam, but do not typically modify the polarization, except for polarizing beam splitters. For example, mirrors, cube corners and retroreflectors are attached to objects that move in order to keep the weight down on the moving object (instead of mounting the interferometer on the moving object).

  • Mirrors are usually attached to the moving object to reflect the beam back into the interferometer, but they can also be used to arbitrarily bend the beam.
  • Cube corners reflect, or return, the laser beam parallel to the incoming path. They cannot be used to control the angle of reflection. The angle of reflection is fixed so that the outgoing beam is parallel to the incoming beam. Cube corners have no housing.
  • Retroreflectors are the same as cube corners, but come with a housing.
  • Beam benders usually deflect the beam at angles, such as 90 degrees.
  • Manipulators are a special category of beam benders. They allow the beam to be easily translated or angled and give more precise control over the beam position.
  • Beam splitters divide a laser beam into multiple beams. The listed percentage tells you the percentage of power of the beam that is split off of the main path. The split path is typically at 90 degrees to the main path.
  • Polarizing beam splitters separate the two frequencies of the laser beam into a reference and a measurement path. Beam power is split equally between the two paths.
  • Vacuum compatible means that the optic has been designed to minimize outgassing and will function in a vacuum environment. Vacuum compatible optics are primarily used in Ebeam direct write applications where the entire exposing machine and positioning stage must be placed in a vacuum.

If you do not see what you are looking for, please use the Contact Us link in the upper right hand corner of this page so that we can discuss custom optics.

  • 10567A 50% Dual Beam Splitter 10567A 50% Dual Beam Splitter 

    10567A 50% Dual Beam Splitter

    The Keysight 10567A dual beam splitter allows both split beams to return through the splitter, parallel to the incoming beam. It is mounted and designed for beam diameters of 6 mm or less

  • 10700A 33% Beam Splitter 10700A 33% Beam Splitter 

    10700A 33% Beam Splitter

    The Keysight 10700A 33% beam splitter is mounted and designed for beam diameters of 6 mm or less.

  • 10701A 50% Beam Splitter 10701A 50% Beam Splitter 

    10701A 50% Beam Splitter

    The Keysight 10701A beam splitter is mounted and is for beam diameters of 6 mm or less.

  • 10703A Retroreflector 10703A Retroreflector 

    10703A Retroreflector

    The Keysight 10703A retroreflector (cube corner) is a basic measurement reflector for linear measurements. It is mounted and designed for beam diameters of 6 mm or less

  • 10704A Retroreflector 10704A Retroreflector 

    10704A Retroreflector

    The Keysight 10704A retroreflector (cube corner) reflector is a measurement reflector for single-beam measurements. It is mounted and designed for beam diameters of 9 mm or less.

  • 10707A Beam Bender 10707A Beam Bender 

    10707A Beam Bender

    The Keysight 10707A bends the incoming beam at a 90-degree angle. It is mounted and designed for beam diameters of 6 mm or less.

  • 10710A Adjustable Mount 10710A Adjustable Mount 

    10710A Adjustable Mount

    The Keysight 10710A adjustable optics mount makes alignment faster and easier. For 10700A, 10701A, 10705A, 10707A. Allows ± 8 degrees tilt and yaw.

  • 10710B Adjustable Mount 10710B Adjustable Mount 

    10710B Adjustable Mount

    The Keysight 10710B adjustable optics mount makes alignment faster and easier. For 10700A, 10701A, 10705A, 10707A. Allows ± 8 degrees tilt and yaw.

  • 10711A Adjustable Mount 10711A Adjustable Mount 

    10711A Adjustable Mount

    The Keysight 10711A adjustable optics mount makes alignment faster and easier. For 10702A, 10706A, 10715A, 10716A. Allows ± 5 degrees tilt and yaw

  • 10713B 1-Inch Cube Corner 10713B 1-Inch Cube Corner 

    10713B 1-Inch Cube Corner

    The Keysight 10713B 1-inch cube corner (retroreflector) can be used as the measurement reflector for linear measurements. This bare optic requires a user supplied mount.

  • 10713C 1/2-Inch Cube Corner 10713C 1/2-Inch Cube Corner 

    10713C 1/2-Inch Cube Corner

    The Keysight 10713C 1/2 inch cube corner reflector can be used as the measurement reflector for linear measurements. This bare optic requires a user supplied mount.

  • 10713D 1/4-Inch Cube Corner 10713D 1/4-Inch Cube Corner 

    10713D 1/4-Inch Cube Corner

    The Keysight 10713D 1/4 inch cube corner (retroreflector) can be used as the measurement reflector for linear measurements. This bare optic requires a user supplied mount.

  • 10722A Plane Mirror Converter 10722A Plane Mirror Converter 

    10722A Plane Mirror Converter

    The Keysight 10722A plane mirror converter modifies the 10702A linear interferometer to function as a plane mirror interferometer. Primarily used in calibrator systems.

  • 10723A High-Stability Adapter 10723A High-Stability Adapter 

    10723A High-Stability Adapter

    The Keysight 10723A High-Stability Adapter is used to convert a 10706A interferometer to a 10706B. Improves thermal stability.

  • 10724A Plane Mirror Reflector 10724A Plane Mirror Reflector 

    10724A Plane Mirror Reflector

    The Keysight 10724A plane mirror reflector is used with the Keysight 10706A/B, 10715A, 10716A and 10737L/R. Can only be used for single axis linear measurements.

  • 10725A 50% Beam Splitter 10725A 50% Beam Splitter 

    10725A 50% Beam Splitter

    The Keysight 10725A 50% beam splitter is designed for beam diameters of 9 mm or less. This bare optic requires a user supplied mount.

  • 10725B 4% Beam Splitter 10725B 4% Beam Splitter 

    10725B 4% Beam Splitter

    The Keysight 10725B 4% beam splitter is designed for beam diameters of 9 mm or less. This bare optic requires a user supplied mount.

  • 10725C 15% Beam Splitter 10725C 15% Beam Splitter 

    10725C 15% Beam Splitter

    The 10725C 15% beam splitter, designed for beam diameters of 9 mm or less, reflects 15% of the total incoming laser beam and transmits 85% straight through. This optic is without housing and requires a user-supplied mount.

  • 10726A Beam Bender 10726A Beam Bender 

    10726A Beam Bender

    The Keysight 10726A bends the incoming beam at a 90-degree angle and is designed for beam diameters of 9 mm or less. This bare optic requires a user supplied mount.

  • 10728A Plane Mirror 10728A Plane Mirror 

    10728A Plane Mirror

    The Keysight 10728A plane mirror is a normal incidence plane mirror for beam diameters of 9mm or less. This bare optic requires a user supplied mount.

  • 10769B Turning Mirror on Universal Mount 10769B Turning Mirror on Universal Mount 

    10769B Turning Mirror on Universal Mount

    The Keysight 10769B turning mirror on universal mount deflects a laser beam at any angle, in either the vertical or horizontal polarization plane. Primarily used in calibrator systems.

  • 10784A Base for Optics Height Adjuster and Post 10784A Base for Optics Height Adjuster and Post 

    10784A Base for Optics Height Adjuster and Post

    The Keysight 10784A Base for Optics Height Adjuster and Post provides a mounting plate for the 10785A Height Adjuster and Post.

  • E1834E 33% Beam Splitter - BK7, fixed horizontal-bend mount E1834E 33% Beam Splitter - BK7, fixed horizontal-bend mount 

    E1834E 33% Beam Splitter - BK7, fixed horizontal-bend mount

    The E1834E is a 33% beam splitter in a high performance horizontal mount that offer the high pointing stability for Keysight laser interferometer measurement system.

  • E1834G 50% Beam Splitter – BK7, fixed horizontal-bend mount E1834G 50% Beam Splitter – BK7, fixed horizontal-bend mount 

    E1834G 50% Beam Splitter – BK7, fixed horizontal-bend mount

    The E1834G is a 50% beam splitter in a high performance horizontal mount that offer the high pointing stability for Keysight laser interferometer measurement system.

  • E1834J 67% Beam Splitter – BK7, fixed horizontal-bend mount E1834J 67% Beam Splitter – BK7, fixed horizontal-bend mount 

    E1834J 67% Beam Splitter – BK7, fixed horizontal-bend mount

    The E1834J is a 67% beam splitter in a high performance horizontal mount that offer the high pointing stability for Keysight laser interferometer measurement system.

  • E1834M Beam Bender – BK7, fixed horizontal-bend mount E1834M Beam Bender – BK7, fixed horizontal-bend mount 

    E1834M Beam Bender – BK7, fixed horizontal-bend mount

    The E1834M is a beam bender that bends the incoming beam at a 90-degree angle and is designed for beam diameters of 9 mm or less.

  • E1834Z Beam Bender – BK7, fixed vertical-bend mount E1834Z Beam Bender – BK7, fixed vertical-bend mount 

    E1834Z Beam Bender – BK7, fixed vertical-bend mount

    The E1834Z is a beam bender that bends the incoming beam at a 90-degree angle and is designed for beam diameters of 9 mm or less.

  • N1206T Manipulator Adjustment Tool Kit N1206T Manipulator Adjustment Tool Kit 

    N1206T Manipulator Adjustment Tool Kit

    The Keysight beam manipulators precisely bend or translate a laser beam. The precise bending and translating results in a properly aligned laser beam and minimizes Abbé and cosine errors.