Choose a country or area to see content specific to your location
솔루션 개요
Accelerating Characterization of 5G mmWave Components
Beamforming is a key technology in 5G communication systems that enables reliable and efficient communications in the 5G Frequency Range 2 (FR2) mmWave band. It is a technique that focuses a wireless signal towards a specific receiving device, rather than have the signal spread in all directions. The resulting direct connection is faster and more reliable than it would be without beamforming.
The beamformer IC is a multiport module device that integrates multidirectional Tx / Rx blocks into an RF front-end that connects to several antennas. These blocks include phase shifters, step attenuators, power amplifiers (PAs), and low noise amplifiers (LNAs). Future ICs will also incorporate frequency converters.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.