#
# (C) Copyright 2000-2004
# Wolfgang Denk, DENX Software Engineering, wd@denx.de.
#
# (C) Copyright 2004
# ARM Ltd.
# Philippe Robin, <philippe.robin@arm.com>
#
# See file CREDITS for list of people who contributed to this
# project.
#
# This program is free software; you can redistribute it and/or
# modify it under the terms of the GNU General Public License as
# published by the Free Software Foundation; either version 2 of
# the License, or (at your option) any later version.
#
# This program is distributed in the hope that it will be useful,
# but WITHOUT ANY WARRANTY; without even the implied warranty of
# MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
# GNU General Public License for more details.
#
# You should have received a copy of the GNU General Public License
# along with this program; if not, write to the Free Software
# Foundation, Inc., 59 Temple Place, Suite 330, Boston,
# MA 02111-1307 USA
#

include $(TOPDIR)/config.mk

LIB	= lib$(BOARD).a

OBJS	:= p500_board.o p500_smi_flash.o p500_uart_hal.o p500_serial.o p500_ether.o p500_hal_ether.o p500_interrupts.o test.o nand.o p500_spi_fpga.o p500_splash.o p500_rtc.o
SOBJS	:= p500_lowlevel_init.o p500_pll.o p500_mt47h32m16_37e.166_cl4.o

$(LIB):	$(OBJS) $(SOBJS)
	$(AR) crv $@ $^

clean:
	rm -f $(SOBJS) $(OBJS)

distclean:	clean
	rm -f $(LIB) core *.bak .depend

#########################################################################

.depend:	Makefile $(SOBJS:.o=.S) $(OBJS:.o=.c)
		$(CC) -M $(CPPFLAGS) $(SOBJS:.o=.S) $(OBJS:.o=.c) > $@

-include .depend

#########################################################################