Sample Programs for B2900
The sample folder contains sample programs for the Agilent B2900 series Precision Source/Measure Unit. Copy all of the sample programs to your hard disk before use.
There are three sweep measurement sample programs written in the following programming languages:- C# with VISA-COM
- National Instruments LabVIEW with VISA-COM
- Microsoft Excel with VISA-COM
The sample programs are protected by copyright. You have a royalty-free right to use, modify, reproduce and distribute the sample programs (and/or any modified version) in any way you find useful, provided that you agree that Agilent has no warranty, obligations, or liability for any sample programs.
Agilent Technologies provides programming samples for illustration only. All sample programs assume that you are familiar with the programming language being demonstrated and the tools used to create and debug procedures. Agilent support engineers can help explain the functionality of Agilent software components and associated commands, but they will not modify these sample programs to provide added functionality or construct procedures to meet your specific needs.
LabVIEW is a U.S. registered trademark of National Instruments Corporation.
Microsoft is a U.S. registered trademark of Microsoft Corporation.
Copyright Agilent Technologies, Inc. 2011
All rights reserved.