Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

P-Series Power Meter Firmware Upgrade

Applicable for N1911A and N1912A power meters.

Compatibility: P-Series N1911A and N1912A power meters.

Please note that after the firmware is installed into the power meter an additional digit will be added to the firmware revision. The number added after the first letter in the firmware revision will designate the number of power sensor channels in the power meter. For example the A.05.04 firmware installed in a two channel N1912A will now be shown as A2.05.04 on the display of the power meter; installed in a one channel N1911A the firmware revision will be A1.05.04.

NOTE: Power meter with the serial number MY58410000 and above, SG58410000 and above will only support firmware version of A.06.01 and above.

Дата выпуска Версия Описание версии
2018-12-07 A.06.01 P-Series Firmware A.06.01.exe

Как загрузить

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Как установить

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Лицензии

  • Лицензия не требуется

Сопроводительная документация

Дополнительное ПО/утилиты

Загрузить

Устанавливается на:

Instrument

Предварительные условия

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Поддерживаемые приборы

  • N1911A, N1912A