Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

P-Series Power Meter Firmware Upgrade

Applicable for N1911A and N1912A power meters.

Compatibility: P-Series N1911A and N1912A power meters.

Please note that after the firmware is installed into the power meter an additional digit will be added to the firmware revision. The number added after the first letter in the firmware revision will designate the number of power sensor channels in the power meter. For example the A.05.04 firmware installed in a two channel N1912A will now be shown as A2.05.04 on the display of the power meter; installed in a one channel N1911A the firmware revision will be A1.05.04.

NOTE: Power meter with the serial number MY58410000 and above, SG58410000 and above will only support firmware version of A.06.01 and above.

Data de lançamento Versão Descrição da Versão
2018-12-07 A.06.01 P-Series Firmware A.06.01.exe

Como Baixar

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Como Instalar

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Licenciamento

  • Não Requer Licença

Documentação de suporte

Software / Utilitários Complementares

Download

Instale em:

Instrument

Pré-requisitos

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Instrumentos Compatíveis

  • N1911A, N1912A