Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

P-Series Power Meter Firmware Upgrade

Applicable for N1911A and N1912A power meters.

Compatibility: P-Series N1911A and N1912A power meters.

Please note that after the firmware is installed into the power meter an additional digit will be added to the firmware revision. The number added after the first letter in the firmware revision will designate the number of power sensor channels in the power meter. For example the A.05.04 firmware installed in a two channel N1912A will now be shown as A2.05.04 on the display of the power meter; installed in a one channel N1911A the firmware revision will be A1.05.04.

NOTE: Power meter with the serial number MY58410000 and above, SG58410000 and above will only support firmware version of A.06.01 and above.

Release Date Version Version Description
2018-12-07 A.06.01 P-Series Firmware A.06.01.exe

How to Download

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

How to Install

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Prerequisites

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Supported Instruments

  • N1911A, N1912A