Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

P-Series Power Meter Firmware Upgrade

Applicable for N1911A and N1912A power meters.

Compatibility: P-Series N1911A and N1912A power meters.

Please note that after the firmware is installed into the power meter an additional digit will be added to the firmware revision. The number added after the first letter in the firmware revision will designate the number of power sensor channels in the power meter. For example the A.05.04 firmware installed in a two channel N1912A will now be shown as A2.05.04 on the display of the power meter; installed in a one channel N1911A the firmware revision will be A1.05.04.

NOTE: Power meter with the serial number MY58410000 and above, SG58410000 and above will only support firmware version of A.06.01 and above.

Date de mise en circulation Version Description de la version
2018-12-07 A.06.01 P-Series Firmware A.06.01.exe

Comment télécharger

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Comment installer

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Logiciels additionels/utilités

Téléchargez

S'installe sur:

Instrument

Préalables

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

Instruments appuyés

  • N1911A, N1912A