N1930B 物理层测试系统软件
全新的物理层测试系统(PLTS)2019 版软件是对高速互连器件(例如电缆、背板、PCB 和连接器)进行信号完整性测量和数据后期处理的行业标准解决方案。全球许多信号完整性实验室已经在研发原型测试阶段使用 PLTS 并受益匪浅。PLTS 2019 现在包括电源完整性测量,支持通过串联方法和并联方法进行电源平面测量。在使用 E5061B VNA 进行低频配电网络(PDN)测量时,利用 PLTS 的对数-对数绘图和 L-C 曲线拟合功能,测量将变得快速而轻松。
- The N1930xB trial license will enable all features N19303B /5B/ 6B/ 7B
发布日期 | 版本 | 版本说明 |
免费试用 |
---|---|---|---|
2021-02-08 | PLTS 2021 | PLTS 2021 Update 1 |
如何下载
- Click on “Download” button indicated on Keysight website
如何安装
- When Install wizard launches, just click install and make sure to use all standard default settings (no custom settings should be used).
- After installation, the first time PLTS launches, it will ask for the license file. Just browse to your location that you saved the license file to and double click on license file.
- The program will then automatically start working properly. Sample s-parameter data files can be found under install folder labelled “Data” that is by standard default located here: This PC OSDisk (C:) > Program Files > Keysight > PLTS2021 > Data
颁发许可证
- 要求具有许可证
- 申请免费试用许可证