这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

2000 和 3000 InfiniiVision X 系列示波器 IVI 和 MATLAB 仪器驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.

Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
 

Current Version Details
Version 1.1.6.0
Models Supported DSO-X 2002A, DSO-X 2004A, DSO-X 2012A, DSO-X 2014A, DSO-X 2022A, DSO-X 2024A, MSO-X 2002A, MSO-X 2004A, MSO-X 2012A, MSO-X 2014A, MSO-X 2022A, MSO-X 2024A, DSO-X 3014A, DSO-X 3024A, DSO-X 3032A, DSO-X 3034A, DSO-X 3052A, DSO-X 3054A, MSO-X 3012A, MSO-X 3014A, MSO-X 3024A, MSO-X 3032A, MSO-X 3034A, MSO-X 3052A, MSO-X 3054A, DSO-X 3012A, MSO-X 3102A, MSO-X 3104A, DSO-X 3102A, DSO-X 3104A
IO Libraries Required Version 16.0 or greater
Driver Types and Version IVI-C (32-bit/64-bit)
IVI-COM (32-bit/64-bit)
MATLAB (32-bit)
IVI Classes Supported IviScope 4.1
IviDriver 1.0
Minimum IVI Shared Components Version 2.2.1.0 
发布日期 版本 版本说明
2019-01-08 2.5.8.0 Added support for C7312, C7312C, C7314, C7314C, C7322, C7322C, C7324, C7324C, C7332, C7332C, C7334, C7334C, C7352, C7352C, C7354, C7354C, C7302, C7302C, C7304 and C7304C models

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (IVI-COM: 32-bit only, IVI-C: 32-bit/64-bit)

IVI class support: IviDriver 1.0, IviScope 4.1

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2018-04-26 2.4.6.0 Added support for P924x series models, modified infiniiVisionVisaSession.cpp file and updated AgInfiniiVision_LabVIEW_WaveformAcq example code.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (IVI-COM: 32-bit only, IVI-C: 32-bit/64-bit)

IVI class support: IviDriver 1.0, IviScope 4.1

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2017-04-20 2.3.9.0 Added support for 1000X series models, added interfaces IAgInfiniiVision8AnalogBus and IAgInfiniiVision8FRA, updated IAgInfiniiVisionExternal2 and IAgInfiniiVisionTrigger5

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (IVI-COM: 32-bit only, IVI-C: 32-bit/64-bit)

IVI class support: IviDriver 1.0, IviScope 4.1

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2015-10-29 2.1.9.0 See description below

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviScope 4.1

Version description:

Added support for 6000x series models which includes
Added new interface(s):

-SEARch5:SERial4:CAN2
-SEARch5:SERial4:LIN2
-SerialBuses4:CAN3
-SerialBuses4:LIN2
-SerialBuses4:SENT2:Trigger2
-WaveGens2
-WaveGens2:Tracking2
-SerialBuses4:CAN3::FD2

Updated the following interfaces with new commands, Enum and Help
-Display4
-MathFunctions2
-Histogram
-SerialBuses4
-Search5

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2015-02-21 2.1.6.0 See description below

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviScope 4.1

Version description:

  • Added support for 3000T series models
  • Added new interface(s):
    • FFT
    • Search4::Serial3::SENT
    • SerialBuses3::SENT
    • SerialBuses3CAN::FD
    • Waveform2
    • System4
    • Display4
  • Updated the following interfaces with new commands
    • Measurements3
    • MathFunctions2

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer
     

颁发许可证

  • 不要求具有许可证

支持文档

2014-05-30 2.0.3.0 Added support for DSO-X/MSO-X 6000 Oscilloscopes, which required changes to some interfaces; see readme for details.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviScope 4.1
 

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer
     

颁发许可证

  • 不要求具有许可证

支持文档

2013-07-19 1.2.8.0 Defect fixes, added new repeated capabilities for MathFunction, WaveGen, new repeated capability names for DigitalChannel and Measurement interfaces, new and updated interfaces...

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2013-05-14 1.1.9.0 Modified the implementation of FetchDigitalWaveform and ReadDigitalWaveform. Modified the enum members for TriggerType enum for IVI-C.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2012-11-13 1.1.8.0 Added support for MSO-X/DSO-X 4000 series

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2012-09-22 1.1.6.0 IviScope 4.1 support, added support for the following models: MSO-X 3102A, MSO-X 3104A, DSO-X 3102A, DSO-X 3104A, updated implementation of Statistics => GetResults method to be able to read measurement data with spaces.

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • DSO-X 2002A, DSO-X 2004A, DSO-X 2012A, DSO-X 2014A, DSO-X 2022A, DSO-X 2024A, MSO-X 2002A, MSO-X 2004A, MSO-X 2012A, MSO-X 2014A, MSO-X 2022A, MSO-X 2024A, DSO-X 3014A, DSO-X 3024A, DSO-X 3032A, DSO-X 3034A, DSO-X 3052A, DSO-X 3054A, MSO-X 3012A, MSO-X 3014A, MSO-X 3024A, MSO-X 3032A, MSO-X 3034A, MSO-X 3052A, MSO-X 3054A, DSO-X 3012A, MSO-X 3102A, MSO-X 3104A, DSO-X 3102A, DSO-X 3104A

相关链接

2011-12-19 1.1.4.0 IVI, MATLAB Version 1.1.4.0 for 2000, 3000 InfiniiVision X-Series Oscilloscopes

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • DSO X 2002A, DSO X 2004A, DSO X 2012A, DSO X 2014A, DSO X 2022A, DSO X 2024A, MSO X 2002A, MSO X 2004A, MSO X 2012A, MSO X 2014A, MSO X 2022A, MSO X 2024A, DSO X 3014A, DSO X 3024A, DSO X 3032A, DSO X 3034A, DSO X 3052A, DSO X 3054A, MSO X 3012A, MSO X 3014A, MSO X 3024A, MSO X 3032A, MSO X 3034A, MSO X 3052A, MSO X 3054A, DSO X 3012A

相关链接

2011-03-03 1.0.8.0 IVI, MATLAB Version 1.0.8.0 for 2000, 3000 InfiniiVision X-Series Oscilloscopes

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • DSO X 2002A, DSO X 2004A, DSO X 2012A, DSO X 2014A, DSO X 2022A, DSO X 2024A, MSO X 2002A, MSO X 2004A, MSO X 2012A, MSO X 2014A, MSO X 2022A, MSO X 2024A, DSO X 3014A, DSO X 3024A, DSO X 3032A, DSO X 3034A, DSO X 3052A, DSO X 3054A, MSO X 3012A, MSO X 3014A, MSO X 3024A, MSO X 3032A, MSO X 3034A, MSO X 3052A, MSO X 3054A, DSO X 3012A

相关链接

2011-02-23 1.0.7.0 IVI, MATLAB Version 1.0.7.0 for 2000, 3000 InfiniiVision X-Series Oscilloscopes

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • DSO X 2002A, DSO X 2004A, DSO X 2012A, DSO X 2014A, DSO X 2022A, DSO X 2024A, MSO X 2002A, MSO X 2004A, MSO X 2012A, MSO X 2014A, MSO X 2022A, MSO X 2024A, DSO X 3014A, DSO X 3024A, DSO X 3032A, DSO X 3034A, DSO X 3052A, DSO X 3054A, MSO X 3012A, MSO X 3014A, MSO X 3024A, MSO X 3032A, MSO X 3034A, MSO X 3052A, MSO X 3054A, DSO X 3012A

相关链接