Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

N6854A Geolocation Server and N6841A RF Sensor Software

The N6854A Geolocation server software and the N6841A RF Sensor software are combined into one downloadable image. This software provides an easy way to configure all of the RF Sensors in your network. It provides diagnostic and firmware update tools, along with a color coded health status indicator for each sensor. Easily upload and geo-align maps to show sensor placement and geolocation results via a heat-map overlay, pinpointing the location of unknown RF emitters. Create launchers to quickly start software applications on one or multiple sensors at the same time. The Geolocation server software is tightly integrated with the N6820ES Surveyor 4D software making a powerful spectrum monitoring and emitter location system.

Included in this software package is the following:

  • Sensor Management Tool (SMT)
  • Sensor Planning and Optimization Tool (SPOT)
  • Sensor Access Library (SAL)
  • Sensor Management Server (SMS)
  • Geolocation Server Software (GSS)

Geolocation measurements require the following:

  • A license for the N6854A Geolocation Server software
  • A minimum of 3 N6841A RF Sensors.
  • N6841A-GFP option for each N6841A RF Sensor used in the Geolocation measurement.
Дата выпуска Версия Описание версии
2019-06-01 2.2.0 Supports FieldFox as a frequency extender, GPS enhancements and pulse measurements for drone detection and location. (See Release Notes for more information).

Как загрузить

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

Как установить

  • Right click on the executable file you downloaded above and select "Run as Administrator" to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Лицензии

Сопроводительная документация

Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7
  • Window 10

Предварительные условия

  • Информация недоступна

Поддерживаемые приборы

  • N6841A, N6854A
2017-09-15 2.1.0 Improved lookback and edge detection algorithms

Как загрузить

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

Как установить

  • Right click on the executable file you downloaded above and select “Run as Administrator” to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Лицензии

Сопроводительная документация

Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7
  • Window 10

Предварительные условия

  • A license for the N6854A Geolocation Server software
  • A minimum of 3 N6841A RF Sensors.
  • N6841A-GFP option for each N6841A RF Sensor used in the Geolocation measurement.
     

Поддерживаемые приборы

  • N6841A, N6854A
2016-09-16 2.0.6 Added Embedded Apps infrastructure, bug fixes, Windows 10 support

Added Embedded Apps infrastructure, bug fixes, Windows 10 support

Как загрузить

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

Как установить

  • Right click on the executable file you downloaded above and select “Run as Administrator” to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Лицензии

Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 8
  • Windows 7
  • Window 10

Предварительные условия

  • None

Поддерживаемые приборы

  • N6841A
2015-10-01 2.0.5 Support of multiple narrowband channels.

Как загрузить

  • Click Download button.
     

Как установить

  • If asked to reboot, reboot and re-run installer until installation is completed.

Лицензии

  • Требуется лицензия
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 8
  • Windows 7

Предварительные условия

  • None

Поддерживаемые приборы

  • N6841A N6854A
2015-02-10 2.0.4 Zoom in/out and multiple measurement averaging within the Sensor Management Tool. Geolocation database backup/restore/clear. Field Strength API calculation. New licensing scheme via Keysight Software Manager.

Как загрузить

  • Click Download button.
     

Как установить

  • If asked to reboot, reboot and re-run installer until installation is completed.

Лицензии

  • Требуется лицензия
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 8
  • Windows 7

Предварительные условия

  • None

Поддерживаемые приборы

  • N6841A N6854A
2014-04-21 2.0.3 This software/firmware includes a driver for a 3rd party frequency extender and adds new geolocation API functions. It also improves frequency tracking and overall reliability.

Как загрузить

  • Click download button

Как установить

  • If asked to reboot, do not reboot until the very end.

Лицензии

  • Требуется лицензия
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7

Предварительные условия

  • Информация недоступна

Поддерживаемые приборы

  • N6841A
2013-04-15 2.02 This software/firmware/FPGA upgrade improves overall reliability as well as time-stamping, phase of data, geo-location algorithm improvements and installer fixes.

Как загрузить

  • Click Download button.
     

Как установить

  • Run the .iso file.

Лицензии

  • Требуется лицензия
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7
  • Windows XP

Предварительные условия

  • None

Поддерживаемые приборы

  • N6841A
2011-01-19 2.0.1 Software file available for download...

Как загрузить

  • Click download button.
     

Как установить

  • Run the .iso file.

Лицензии

  • Требуется лицензия
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7
  • Windows XP

Предварительные условия

  • None

Поддерживаемые приборы

  • N6841A