Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

N6854A Geolocation Server and N6841A RF Sensor Software

The N6854A Geolocation server software and the N6841A RF Sensor software are combined into one downloadable image. This software provides an easy way to configure all of the RF Sensors in your network. It provides diagnostic and firmware update tools, along with a color coded health status indicator for each sensor. Easily upload and geo-align maps to show sensor placement and geolocation results via a heat-map overlay, pinpointing the location of unknown RF emitters. Create launchers to quickly start software applications on one or multiple sensors at the same time. Develop your own applications using the sensor access library and example programs.

Included in this software package is the following:

  • Sensor Management Tool (SMT)
  • Sensor Planning and Optimization Tool (SPOT)
  • Sensor Access Library (SAL)
  • Sensor Management Server (SMS)
  • Geolocation Server Software (GSS)

Geolocation measurements require the following:

  • A license for the N6854A Geolocation Server software
  • A minimum of 3 N6841A RF Sensors.
  • N6841A-GFP option for each N6841A RF Sensor used in the Geolocation measurement.
Release Date Version Version Description
2019-06-01 2.2.0 Supports FieldFox as a frequency extender, GPS enhancements and pulse measurements for drone detection and location. (See Release Notes for more information).

How to Download

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

How to Install

  • Right click on the executable file you downloaded above and select "Run as Administrator" to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Licensing

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Window 10

Prerequisites

  • Information Not Available

Supported Instruments

  • N6841A, N6854A