Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

N6854A Geolocation Server and N6841A RF Sensor Software

The N6854A Geolocation server software and the N6841A RF Sensor software are combined into one downloadable image. This software provides an easy way to configure all of the RF Sensors in your network. It provides diagnostic and firmware update tools, along with a color coded health status indicator for each sensor. Easily upload and geo-align maps to show sensor placement and geolocation results via a heat-map overlay, pinpointing the location of unknown RF emitters. Create launchers to quickly start software applications on one or multiple sensors at the same time. Develop your own applications using the sensor access library and example programs.

Included in this software package is the following:

  • Sensor Management Tool (SMT)
  • Sensor Planning and Optimization Tool (SPOT)
  • Sensor Access Library (SAL)
  • Sensor Management Server (SMS)
  • Geolocation Server Software (GSS)

Geolocation measurements require the following:

  • A license for the N6854A Geolocation Server software
  • A minimum of 3 N6841A RF Sensors.
  • N6841A-GFP option for each N6841A RF Sensor used in the Geolocation measurement.
Date de mise en circulation Version Description de la version
2017-09-15 2.1.0 Improved lookback and edge detection algorithms

Comment télécharger

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

Comment installer

  • Right click on the executable file you downloaded above and select “Run as Administrator” to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Autorisation d'exploitation

Document d'appui

Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7
  • Window 10

Préalables

  • A license for the N6854A Geolocation Server software
  • A minimum of 3 N6841A RF Sensors.
  • N6841A-GFP option for each N6841A RF Sensor used in the Geolocation measurement.
     

Instruments appuyés

  • N6841A, N6854A
2016-09-16 2.0.6 Added Embedded Apps infrastructure, bug fixes, Windows 10 support

Added Embedded Apps infrastructure, bug fixes, Windows 10 support

Comment télécharger

  • Click the Download button
  • Follow the on-screen instructions and save the executable file to your computer hard drive

Comment installer

  • Right click on the executable file you downloaded above and select “Run as Administrator” to install
  • Follow the on-screen instructions to complete the installation. If asked to reboot, reboot and re-run installer until installation is completed

Autorisation d'exploitation

Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 8
  • Windows 7
  • Window 10

Préalables

  • None

Instruments appuyés

  • N6841A
2015-10-01 2.0.5 Support of multiple narrowband channels.

Comment télécharger

  • Click Download button.
     

Comment installer

  • If asked to reboot, reboot and re-run installer until installation is completed.

Autorisation d'exploitation

  • Requiert une licence
2015-02-10 2.0.4 Zoom in/out and multiple measurement averaging within the Sensor Management Tool. Geolocation database backup/restore/clear. Field Strength API calculation. New licensing scheme via Keysight Software Manager.

Comment télécharger

  • Click Download button.
     

Comment installer

  • If asked to reboot, reboot and re-run installer until installation is completed.

Autorisation d'exploitation

  • Requiert une licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 8
  • Windows 7

Préalables

  • None

Instruments appuyés

  • N6841A N6854A
2014-04-21 2.0.3 This software/firmware includes a driver for a 3rd party frequency extender and adds new geolocation API functions. It also improves frequency tracking and overall reliability.

Comment télécharger

  • Click download button

Comment installer

  • If asked to reboot, do not reboot until the very end.

Autorisation d'exploitation

  • Requiert une licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7

Préalables

  • Information non-disponible

Instruments appuyés

  • N6841A
2013-04-15 2.02 This software/firmware/FPGA upgrade improves overall reliability as well as time-stamping, phase of data, geo-location algorithm improvements and installer fixes.

Comment télécharger

  • Click Download button.
     

Comment installer

  • Run the .iso file.

Autorisation d'exploitation

  • Requiert une licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7
  • Windows XP

Préalables

  • None

Instruments appuyés

  • N6841A
2011-01-19 2.0.1 Software file available for download...

Comment télécharger

  • Click download button.
     

Comment installer

  • Run the .iso file.

Autorisation d'exploitation

  • Requiert une licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7
  • Windows XP

Préalables

  • None

Instruments appuyés

  • N6841A