What are you looking for?
The calibration definition file of the 85038A/F/M for the ENA
Overview
The standard definition file of the 85038A/F/M(7-16 Calibration kits) can be imported into the ENA by following procedure.
[E5070B/71B firmware revision A.05.02 or below]
Can not use 85038A/F/M. Please update firmware.
[E5070B/71B firmware revision A.06.00 thru A.06.51]
Please update firmware. If you still want to use these firmware revision, definition file of 85038A/F/M can be loaded to ENA by following procedure.
Step1. Right click the "85038.CKX" listed below then select "save target as...", then save file to the floppy disk.
Step2. Copy the "85038.CKX" to the D drive of the ENA.
Step3. Import the definition file by "Calibration" > "Modify Cal Kit" > "Import cal kit".
[E5070B/71B firmware revision A.08.01 or later]
On the installation of the new firmware, 85038A/F/M is automatically loaded as the 10th of pre-defined cal kit.
However, if the 10th cal kit of ENA is already defined by user, 85038A/F/M will not be overwritten. Please activate 85038A/F/M by following procedure.
Step1. [Cal] > "cal kit" > Select 10th cal kit
Step2. [Cal] > "Modify cal kit" > "Restore Cal Kit" > "OK"
[E5071C firmware revision A.07.01 or A.07.02]
Please update firmware. If you still want to use these firmware revision, definition file of 85038A/F/M can be loaded to ENA by following procedure.
Step1. Right click the "85038.CKX" listed below then select "save target as...", then save file to the USB memory.
Step2. Copy the "85038.CKX" to the D drive of the ENA.
Step3. Import the definition file by "Calibration" > "Modify Cal Kit" > "Import cal kit".
[E5071C firmware revision A.08.01 or later]
On the installation of the new firmware, 85038A/F/M is automatically loaded as the 10th of pre-defined cal kit.
However, if the 10th cal kit of ENA is already defined by user, 85038A/F/M will not be overwritten. Please activate 85038A/F/M by following procedure.
Step1. [Cal] > "cal kit" > Select 10th cal kit
Step2. [Cal] > "Modify cal kit" > "Restore Cal Kit" > "OK"
Release Date | Version | Version Description |
---|---|---|
2006-01-11 | n/a | The calibration definition file of the 85038A/F/M for the ENA |
Release Date | Version |
---|---|
2006-01-11 | n/a |
Version Description |
---|
The calibration definition file of the 85038A/F/M for the ENA |
How to Download
- See Above
How to Install
- See Above
Licensing
- Does Not Require a License
Installs on: Instrument
Operating System
- Windows XP
Prerequisites
- See Above
Supported Instruments
- E5070A, E5071A, E5070B, E5071B, E5071C, E5061A, E5062A